Tech Library Products & Technologies (-) Applications & Cases Solution Guides Facet Tech Note List Article Category » Taxonomy term » Name Absorberkammern und Funkwellen Absorber Application Specific IC (ASIC) Durchsichtige Leitende Folien EMV-Bauelemente HF-Komponenten Induktivitäten (Spulen) Keramische Schalt- / Heizelemente und Piezo-Komponenten, Schütze, Signaltongeber und Mikrofon Kondensatoren Schirmungsfolien / Magnetfolien Schutzbauelemente Sensoren und Sensorsysteme Stromversorgungen Übertrager Facet Tech Note List Product Categories L1 Automobilindustrie ICT Industrie & Energie Medizin & Gesundheitswesen Others Unterhaltungselektronik Wearables Facet Tech Note List Application Category 2023 2022 2021 2020 2019 2018 2017 2016 2015 2014 Facet Tech Note List Published on Date Applications & Cases März. 2023 [Application Note] Temperature sensing of LED Flash with NTC thermistor New The NTC thermistor is a thermally sensitive resistor whose resistance decreases rapidly as the temperature rises. This property can be utilized in various applications such as temperature sensors and thermal protection devices to protect circuits from overheating. By mounting the NTC thermistor in close proximity to the heat source, it can accurately sense the temperature of the heat source. However, in some cases, such as when there are constraints on the size of the board or the pattern layout, it may need to be mounted in a location away from the heat source. In this article, considering such conditions, we used the LEDs on the LED flash circuit board as the heat source and simulated heat generation to check the temperature difference between the LEDs and the NTC thermistors caused by the different mounting positions. We also checked the effect of circuit board thickness. The NTC thermistor is a thermally sensitive resistor whose resistance decreases rapidly as the temperature rises. This property can be utilized in various applications such as temperature sensors and thermal protection devices to protect circuits from overheating. By mounting the NTC thermistor in close proximity to the heat source, it can accurately sense the temperature of the heat source. However, in some cases, such as when there are constraints on the size of the board or the pattern layout, it may need to be mounted in a location away from the heat source. In this article, considering such conditions, we used the LEDs on the LED flash circuit board as the heat source and simulated heat generation to check the temperature difference between the LEDs and the NTC thermistors caused by the different mounting positions. We also checked the effect of circuit board thickness. Schutzbauelemente Temperatursensoren (NTC) SMD-NTC-Thermistoren (Sensoren) Applications & Cases März. 2023 [Application Note] Aluminium-Elektrolyt-Kondensatoren für den DC-Link in Onboard-Chargern New Mit dem wachsenden Markt für elektrifizierte Fahrzeuge (EVs) steigt die Nachfrage nach Onboard-Chargern (OBCs) schnell an. OBCs eröffnen die Möglichkeit, Fahrzeuge nicht nur an Schnellladestationen für Gleichstrom, sondern auch mit Wechselstromquellen in angemessener Zeit aufzuladen. Solche Systeme reichen derzeit bis zu 22 kW mit Betriebsspannungen bis zu 800 V. Die Aufgabe des OBC besteht darin, die Wechselspannung aus einer externen Quelle in eine spezifische Gleichspannung umzuwandeln, die auf den Anforderungen des Batteriemanagement-Systems basiert. Dadurch kann ein batterieschonender und schneller Ladevorgang erreicht werden. Insbesondere in abgelegenen Gebieten ohne ausreichende DC-Schnellladeinfrastruktur sind OBCs unverzichtbar, um die Attraktivität von E-Fahrzeugen zu steigern.Wegen der Komplexität solcher Systeme benötigen OBCs eine gewisse Kapazität, um die Gleichspannung, mit der die Batterie geladen wird, zu stabilisieren. Aluminium-Elektrolyt-Kondensatoren sind hier eine attraktive Lösung, da sie die wichtigsten Anforderungen erfüllen können, wie z. B. hohe Spannungen von bis zu 500 V, große Kapazitäten von bis zu 820 µF und hohe Ripplestrom-Belastbarkeit bei einem Betriebstemperaturbereich von -40 °C bis 105 °C. Mit dem wachsenden Markt für elektrifizierte Fahrzeuge (EVs) steigt die Nachfrage nach Onboard-Chargern (OBCs) schnell an. OBCs eröffnen die Möglichkeit, Fahrzeuge nicht nur an Schnellladestationen für Gleichstrom, sondern auch mit Wechselstromquellen in angemessener Zeit aufzuladen. Solche Systeme reichen derzeit bis zu 22 kW mit Betriebsspannungen bis zu 800 V. Die Aufgabe des OBC besteht darin, die Wechselspannung aus einer externen Quelle in eine spezifische Gleichspannung umzuwandeln, die auf den Anforderungen des Batteriemanagement-Systems basiert. Dadurch kann ein batterieschonender und schneller Ladevorgang erreicht werden. Insbesondere in abgelegenen Gebieten ohne ausreichende DC-Schnellladeinfrastruktur sind OBCs unverzichtbar, um die Attraktivität von E-Fahrzeugen zu steigern.Wegen der Komplexität solcher Systeme benötigen OBCs eine gewisse Kapazität, um die Gleichspannung, mit der die Batterie geladen wird, zu stabilisieren. Aluminium-Elektrolyt-Kondensatoren sind hier eine attraktive Lösung, da sie die wichtigsten Anforderungen erfüllen können, wie z. B. hohe Spannungen von bis zu 500 V, große Kapazitäten von bis zu 820 µF und hohe Ripplestrom-Belastbarkeit bei einem Betriebstemperaturbereich von -40 °C bis 105 °C. Kondensatoren Aluminium-Elektrolyt-Kondensatoren Snap-in, Multi Pin, Large-Size Kondensatoren Applications & Cases Febr. 2023 [Application Note] TDK TVS-Signalintegrität für USB4® und Thunderbolt® 4 – Effektiver ESD-Schutz von High-Speed-Datenleitungen Der Universal Serial Bus (USB) ist ein seit über 20 Jahren etablierter Industriestandard, der das serielle Kommunikationsprotokoll sowie die Anschlüsse, Kabel und Ladegeräte für batteriebetriebene, wiederaufladbare tragbare Geräte definiert. Mit jeder Aktualisierung des USB-Protokolls wurden die Datenraten kontinuierlich erhöht. Die derzeit aktuelle Version ist das USB4® -Protokoll mit Datenraten von bis zu 40 Gbit/s, gefolgt von dem kürzlich veröffentlichten USB Power Delivery (PD) Ladeprotokoll. Diese Entwicklung bedeutete eine Verkürzung der Ladezeit von Peripheriegeräten über den USB-Stecker, obwohl die Akkukapazitäten der Peripheriegeräte immer größer weurden. Die jüngsten Marktentwicklungen, die die Technologietrends zur Unterstützung der Anforderungen vorantreiben, wurden von den Angeboten der Hersteller angeführt, gefolgt von Versuchen zur Standardisierung der verwendeten Geräte. Eine der weit verbreiteten Lösungen, die die oben genannten Anforderungen vereint, ist der USB Type-C® Anschluss, der eine Stromversorgung von bis zu 100 W unterstützt. Der Universal Serial Bus (USB) ist ein seit über 20 Jahren etablierter Industriestandard, der das serielle Kommunikationsprotokoll sowie die Anschlüsse, Kabel und Ladegeräte für batteriebetriebene, wiederaufladbare tragbare Geräte definiert. Mit jeder Aktualisierung des USB-Protokolls wurden die Datenraten kontinuierlich erhöht. Die derzeit aktuelle Version ist das USB4® -Protokoll mit Datenraten von bis zu 40 Gbit/s, gefolgt von dem kürzlich veröffentlichten USB Power Delivery (PD) Ladeprotokoll. Diese Entwicklung bedeutete eine Verkürzung der Ladezeit von Peripheriegeräten über den USB-Stecker, obwohl die Akkukapazitäten der Peripheriegeräte immer größer weurden. Die jüngsten Marktentwicklungen, die die Technologietrends zur Unterstützung der Anforderungen vorantreiben, wurden von den Angeboten der Hersteller angeführt, gefolgt von Versuchen zur Standardisierung der verwendeten Geräte. Eine der weit verbreiteten Lösungen, die die oben genannten Anforderungen vereint, ist der USB Type-C® Anschluss, der eine Stromversorgung von bis zu 100 W unterstützt. Schutzbauelemente TVS-Dioden Applications & Cases Febr. 2023 [Application Note] Failure Modes and Countermeasures in Actual Use of NTC Thermistors NTC (Negative Temperature Coefficient) thermistors are thermally sensitive semiconductor resistors which show a decrease in resistance as temperature increases, and its rate of change is extremely large. Its main applications include temperature sensing in electronic equipment and temperature compensation for module products. However, if the user misuses the product, it may not function properly and, in the worst case, this may cause malfunctions. This page introduces the causes and countermeasures for ”cracks” and ”melting of ceramics” as failure modes caused by improper use of NTC thermistors. NTC (Negative Temperature Coefficient) thermistors are thermally sensitive semiconductor resistors which show a decrease in resistance as temperature increases, and its rate of change is extremely large. Its main applications include temperature sensing in electronic equipment and temperature compensation for module products. However, if the user misuses the product, it may not function properly and, in the worst case, this may cause malfunctions. This page introduces the causes and countermeasures for ”cracks” and ”melting of ceramics” as failure modes caused by improper use of NTC thermistors. Sensoren und Sensorsysteme Temperatursensoren (NTC) SMD-NTC-Thermistoren (Sensoren) Applications & Cases Febr. 2023 Sensors for New Mobility 【How electrification and autonomous driving are expanding the role of sensor technologies within automotive designs】 The automotive production landscape is changing. The proliferation of electronic devices and sensors in modern car design has grown exponentially in recent years. It will expand further as the industry continues its transition toward e-mobility and autonomous driving. The core technologies featured in electric vehicles expand the realm into which sensors are deployed. Also, combustion engine vehicle gas sensors have shifted away from exhaust gas monitoring toward internal air quality (IAQ) measurement. 【How electrification and autonomous driving are expanding the role of sensor technologies within automotive designs】 The automotive production landscape is changing. The proliferation of electronic devices and sensors in modern car design has grown exponentially in recent years. It will expand further as the industry continues its transition toward e-mobility and autonomous driving. The core technologies featured in electric vehicles expand the realm into which sensors are deployed. Also, combustion engine vehicle gas sensors have shifted away from exhaust gas monitoring toward internal air quality (IAQ) measurement. Sensoren und Sensorsysteme Bewegungssensoren / Inertialsensoren Drucksensoren Temperatursensoren (NTC) Ultraschallsensoren Winkelsensoren Drucksensor-Transmitter Embedded Motor-Controller IMU (Inertial Measurement Unit) Luftdrucksensoren MEMS-Mikrofone (Mikrofon) NTC-Elemente NTC-Sensor-Systeme PiezoHapt™ Aktuatoren PowerHap™ Aktuatoren SMD-NTC-Thermistoren (Sensoren) Time-of-Flight (ToF) Ultraschallsensoren TMR Winkelsensoren Applications & Cases Febr. 2023 [Application Note] Common Mode Chokes and Chip Varistors for 10BASE-T1S While the development of next-generation vehicles for fully automated driving is gaining momentum, vehicle architecture is beginning to undergo major changes. Among them, the automotive network that connects ECUs responsible for advanced driver-assistance system (ADAS) is a very important element. One particular focus is on automotive Ethernet for automotive networks, with 100BASE-T1 (100 Mbps) and 1000BASE-T1 (1 Gbps) for sensor systems in cameras, radar, and LiDARs. Furthermore, the 10BASE-T1S, a new standard for automotive Ethernet with a transmission speed of 10 Mbps, is gaining more attention. Sample applications: Possible applications include actuator systems and sensors. While the development of next-generation vehicles for fully automated driving is gaining momentum, vehicle architecture is beginning to undergo major changes. Among them, the automotive network that connects ECUs responsible for advanced driver-assistance system (ADAS) is a very important element. One particular focus is on automotive Ethernet for automotive networks, with 100BASE-T1 (100 Mbps) and 1000BASE-T1 (1 Gbps) for sensor systems in cameras, radar, and LiDARs. Furthermore, the 10BASE-T1S, a new standard for automotive Ethernet with a transmission speed of 10 Mbps, is gaining more attention. Sample applications: Possible applications include actuator systems and sensors. EMV-Bauelemente Chip Varistors / Ceramic Transient Voltage Suppressors Daten- und Signalleitungsdrosseln / Gleichtaktfilter Applications & Cases Jan. 2023 [Application Note] Example of ESD Countermeasures on Actual Equipment | LED Protection with Chip Varistors While smartphones, TWS, and other mobile devices are becoming smaller and more sophisticated, devices and ICs are becoming more vulnerable to electrostatic discharge (ESD), surges, and other types of immunity. These mobile devices are increasingly being hand-held, operated, and worn. Therefore, ESD countermeasures are needed more than ever, while ESD protection components are also increasingly being used to prevent ESD. TDK offers a lineup of chip varistors as components that can protect circuits from ESD. Lastly, using actual devices, this article presents examples of ESD countermeasures using chip varistors for actual failures that occur when ESD enters a device. While smartphones, TWS, and other mobile devices are becoming smaller and more sophisticated, devices and ICs are becoming more vulnerable to electrostatic discharge (ESD), surges, and other types of immunity. These mobile devices are increasingly being hand-held, operated, and worn. Therefore, ESD countermeasures are needed more than ever, while ESD protection components are also increasingly being used to prevent ESD. TDK offers a lineup of chip varistors as components that can protect circuits from ESD. Lastly, using actual devices, this article presents examples of ESD countermeasures using chip varistors for actual failures that occur when ESD enters a device. Chip Varistors / Ceramic Transient Voltage Suppressors Applications & Cases Dez. 2022 [Application Note] Noise Countermeasures and Audio Quality Improvement for Bluetooth Audio Devices In recent years, wireless audio has become more commonplace and even the norm in many of our everyday products. The use of network audio, which does not use conventional media sources such as compact discs (CDs), is also expanding due to the increase in sound source data from high-resolution audio and subscription-based music distribution services. New audio usage is often centered on smartphone-based services that provide audio through the smartphone to speakers and earbuds [earphones, earpods, etc.] via Bluetooth connectivity. These two use cases for audio output have come to dominate. The recent mass implementation of True Wireless Stereo (TWS) within earbuds, with their comfortable cable-free non-tangling fit, has yielded vastly improved sound quality over traditional Bluetooth audio technology. TWS also comes with the ability to cancel external noise (isolation) which results in quieter playback. This feature allows users to use TWS-based devices without concerns of the sound being “broadcasted” to surrounding areas. Additionally, Bluetooth connected speakers, which also do not require cables for signal transmission, allow for unfettered placement of playback devices and speakers. These mobile speakers, with their built-in amplifiers, can operate on battery power and be completely portable. Bluetooth enabled audio devices are easy to use, easy to connect to and have many advantages. However, since they require a wireless signal, they can be susceptible to problems that do not occur with cable-connected audio devices. This article describes phenomena that can cause problems within Bluetooth audio designs and will provide examples of potential countermeasures. In recent years, wireless audio has become more commonplace and even the norm in many of our everyday products. The use of network audio, which does not use conventional media sources such as compact discs (CDs), is also expanding due to the increase in sound source data from high-resolution audio and subscription-based music distribution services. New audio usage is often centered on smartphone-based services that provide audio through the smartphone to speakers and earbuds [earphones, earpods, etc.] via Bluetooth connectivity. These two use cases for audio output have come to dominate. The recent mass implementation of True Wireless Stereo (TWS) within earbuds, with their comfortable cable-free non-tangling fit, has yielded vastly improved sound quality over traditional Bluetooth audio technology. TWS also comes with the ability to cancel external noise (isolation) which results in quieter playback. This feature allows users to use TWS-based devices without concerns of the sound being “broadcasted” to surrounding areas. Additionally, Bluetooth connected speakers, which also do not require cables for signal transmission, allow for unfettered placement of playback devices and speakers. These mobile speakers, with their built-in amplifiers, can operate on battery power and be completely portable. Bluetooth enabled audio devices are easy to use, easy to connect to and have many advantages. However, since they require a wireless signal, they can be susceptible to problems that do not occur with cable-connected audio devices. This article describes phenomena that can cause problems within Bluetooth audio designs and will provide examples of potential countermeasures. Entstörfilter Kerbfilter mit ESD-Schutzfunktion Applications & Cases Nov. 2022 [Application Note] Sensors for Drones TDK offers a full suite of sensors that are perfectly suited for drones of all types from consumer/prosumer models to industrial units. In just a few years, drones have become indispensable in one application after another, including such diverse areas as agriculture, real estate and cinematography. For all this success, drones still have almost unlimited potential given their suitability for a wide variety of uses including delivery, inspection, search & rescue, monitoring, and mapping, to name just a few. Fundamental to drone utility is sensor technology. Drones rely on diverse sets of sensors for two broad purposes. First for their own functionality, notably flight and navigation, and second, for their ancillary capabilities – cameras for vision, motion detectors to sense activity, heat sensors to detect temperature, and so on. TDK offers a full suite of sensors that are perfectly suited for drones of all types from consumer/prosumer models to industrial units. In just a few years, drones have become indispensable in one application after another, including such diverse areas as agriculture, real estate and cinematography. For all this success, drones still have almost unlimited potential given their suitability for a wide variety of uses including delivery, inspection, search & rescue, monitoring, and mapping, to name just a few. Fundamental to drone utility is sensor technology. Drones rely on diverse sets of sensors for two broad purposes. First for their own functionality, notably flight and navigation, and second, for their ancillary capabilities – cameras for vision, motion detectors to sense activity, heat sensors to detect temperature, and so on. Sensoren und Sensorsysteme Bewegungssensoren / Inertialsensoren Drucksensoren Temperatursensoren (NTC) Ultraschallsensoren Embedded Motor-Controller IMU (Inertial Measurement Unit) Luftdrucksensoren MEMS-Mikrofone (Mikrofon) NTC-Elemente NTC-Sensor-Systeme SMD-NTC-Thermistoren (Sensoren) Time-of-Flight (ToF) Ultraschallsensoren Applications & Cases Okt. 2022 PCB Pattern Design for ESD Countermeasures | ESD Visualization TDK has a lineup of multilayer chip varistors that protect equipment for malfunction and failure due to ESD (electrostatic discharge), and we have long contributed to solving customer ESD problems. Recently, however, although multilayer chip varistors have been effective in the past, they have been unable to provide sufficient protection as customer devices have become smaller, lighter, and more sophisticated. To investigate the cause of this problem, we conducted ESD tests assuming the miniaturization of customer equipment. TDK has a lineup of multilayer chip varistors that protect equipment for malfunction and failure due to ESD (electrostatic discharge), and we have long contributed to solving customer ESD problems. Recently, however, although multilayer chip varistors have been effective in the past, they have been unable to provide sufficient protection as customer devices have become smaller, lighter, and more sophisticated. To investigate the cause of this problem, we conducted ESD tests assuming the miniaturization of customer equipment. Chip Varistors / Ceramic Transient Voltage Suppressors Seitennummerierung Aktuelle Seite 1 Seite 2 Seite 3 Seite 4 Seite 5 … Nächste Seite Next › Letzte Seite Last »