Tech Library Products & Technologies (-) Applications & Cases Solution Guides Facet Tech Note List Article Category » Taxonomy term » Name Durchsichtige Leitende Folien EMV-Bauelemente Induktivitäten (Spulen) Keramische Schalt- / Heizelemente und Piezo-Komponenten, Schütze, Signaltongeber und Mikrofon Kondensatoren Schirmungsfolien / Magnetfolien (-) Schutzbauelemente Sensoren und Sensorsysteme Übertrager Facet Tech Note List Product Categories L1 Automobilindustrie ICT Industrie & Energie Medizin & Gesundheitswesen Others Unterhaltungselektronik (-) Wearables Facet Tech Note List Application Category 2023 2018 2016 Facet Tech Note List Published on Date Applications & Cases März. 2023 [Application Note] Temperature sensing of LED Flash with NTC thermistor New The NTC thermistor is a thermally sensitive resistor whose resistance decreases rapidly as the temperature rises. This property can be utilized in various applications such as temperature sensors and thermal protection devices to protect circuits from overheating. By mounting the NTC thermistor in close proximity to the heat source, it can accurately sense the temperature of the heat source. However, in some cases, such as when there are constraints on the size of the board or the pattern layout, it may need to be mounted in a location away from the heat source. In this article, considering such conditions, we used the LEDs on the LED flash circuit board as the heat source and simulated heat generation to check the temperature difference between the LEDs and the NTC thermistors caused by the different mounting positions. We also checked the effect of circuit board thickness. The NTC thermistor is a thermally sensitive resistor whose resistance decreases rapidly as the temperature rises. This property can be utilized in various applications such as temperature sensors and thermal protection devices to protect circuits from overheating. By mounting the NTC thermistor in close proximity to the heat source, it can accurately sense the temperature of the heat source. However, in some cases, such as when there are constraints on the size of the board or the pattern layout, it may need to be mounted in a location away from the heat source. In this article, considering such conditions, we used the LEDs on the LED flash circuit board as the heat source and simulated heat generation to check the temperature difference between the LEDs and the NTC thermistors caused by the different mounting positions. We also checked the effect of circuit board thickness. Schutzbauelemente Temperatursensoren (NTC) SMD-NTC-Thermistoren (Sensoren) Applications & Cases Febr. 2023 [Application Note] TDK TVS-Signalintegrität für USB4® und Thunderbolt® 4 – Effektiver ESD-Schutz von High-Speed-Datenleitungen Der Universal Serial Bus (USB) ist ein seit über 20 Jahren etablierter Industriestandard, der das serielle Kommunikationsprotokoll sowie die Anschlüsse, Kabel und Ladegeräte für batteriebetriebene, wiederaufladbare tragbare Geräte definiert. Mit jeder Aktualisierung des USB-Protokolls wurden die Datenraten kontinuierlich erhöht. Die derzeit aktuelle Version ist das USB4® -Protokoll mit Datenraten von bis zu 40 Gbit/s, gefolgt von dem kürzlich veröffentlichten USB Power Delivery (PD) Ladeprotokoll. Diese Entwicklung bedeutete eine Verkürzung der Ladezeit von Peripheriegeräten über den USB-Stecker, obwohl die Akkukapazitäten der Peripheriegeräte immer größer weurden. Die jüngsten Marktentwicklungen, die die Technologietrends zur Unterstützung der Anforderungen vorantreiben, wurden von den Angeboten der Hersteller angeführt, gefolgt von Versuchen zur Standardisierung der verwendeten Geräte. Eine der weit verbreiteten Lösungen, die die oben genannten Anforderungen vereint, ist der USB Type-C® Anschluss, der eine Stromversorgung von bis zu 100 W unterstützt. Der Universal Serial Bus (USB) ist ein seit über 20 Jahren etablierter Industriestandard, der das serielle Kommunikationsprotokoll sowie die Anschlüsse, Kabel und Ladegeräte für batteriebetriebene, wiederaufladbare tragbare Geräte definiert. Mit jeder Aktualisierung des USB-Protokolls wurden die Datenraten kontinuierlich erhöht. Die derzeit aktuelle Version ist das USB4® -Protokoll mit Datenraten von bis zu 40 Gbit/s, gefolgt von dem kürzlich veröffentlichten USB Power Delivery (PD) Ladeprotokoll. Diese Entwicklung bedeutete eine Verkürzung der Ladezeit von Peripheriegeräten über den USB-Stecker, obwohl die Akkukapazitäten der Peripheriegeräte immer größer weurden. Die jüngsten Marktentwicklungen, die die Technologietrends zur Unterstützung der Anforderungen vorantreiben, wurden von den Angeboten der Hersteller angeführt, gefolgt von Versuchen zur Standardisierung der verwendeten Geräte. Eine der weit verbreiteten Lösungen, die die oben genannten Anforderungen vereint, ist der USB Type-C® Anschluss, der eine Stromversorgung von bis zu 100 W unterstützt. Schutzbauelemente TVS-Dioden Applications & Cases Okt. 2018 [Application Note] Heiß-kalt kombiniert Leistungsstarke Lasten sind beim Einschalten für Sicherungen und Bauelemente ein großer Stressfaktor, da hierbei sehr hohe Ströme fließen. Um diese zu vermeiden, bietet TDK keramische EPCOS Einschaltstrom-Begrenzer auf der Basis von NTC- und PTC-Thermistoren, die auch kombiniert eingesetzt werden können. Leistungsstarke Lasten sind beim Einschalten für Sicherungen und Bauelemente ein großer Stressfaktor, da hierbei sehr hohe Ströme fließen. Um diese zu vermeiden, bietet TDK keramische EPCOS Einschaltstrom-Begrenzer auf der Basis von NTC- und PTC-Thermistoren, die auch kombiniert eingesetzt werden können. Schutzbauelemente Überlastschutz PTC-Einschaltstrombegrenzer Applications & Cases Mai. 2018 [Application Note] How to Use ESD/surge Protection Devices : SMD Varistors SMD or chip varistors are voltage-dependent resistors based on ceramic multilayer technology. They are widely used to protect electronic circuits in consumer devices and telecom, industrial and automotive applications against transient overvoltages, such as electrostatic discharges (ESD) and surge transients. SMD or chip varistors are voltage-dependent resistors based on ceramic multilayer technology. They are widely used to protect electronic circuits in consumer devices and telecom, industrial and automotive applications against transient overvoltages, such as electrostatic discharges (ESD) and surge transients. Schutzbauelemente Applications & Cases Mai. 2018 [Application Note] The Optimal Applications for Chip Varistors for ESD Countermeasures Chip varistors have both surge absorption capabilities and noise suppressing effects. Chip varistors have both surge absorption capabilities and noise suppressing effects. Schutzbauelemente Applications & Cases Apr. 2018 [Application Note] Chip Varistors Prevent Damage of Electronics from Electrostatic Discharge TDK’s chip varistors in the AVR series, which are made with our own materials, feature high resistance to repeated surges. Products that substitute Zener diodes in compact devices such as solenoid valves and stepping motors, which are rapidly and frequently turned on and off, are also available. TDK’s chip varistors in the AVR series, which are made with our own materials, feature high resistance to repeated surges. Products that substitute Zener diodes in compact devices such as solenoid valves and stepping motors, which are rapidly and frequently turned on and off, are also available. Schutzbauelemente Applications & Cases Apr. 2018 [Application Note] How to Use Temperature Protection Devices : Chip NTC Thermistors NTC thermistors are heat-sensitive resistor elements of which resistance values rapidly decrease with rise of temperature. With this property, they are used as temperature protection devices for protecting circuits from overheating as well as temperature sensors. NTC thermistors are heat-sensitive resistor elements of which resistance values rapidly decrease with rise of temperature. With this property, they are used as temperature protection devices for protecting circuits from overheating as well as temperature sensors. Schutzbauelemente Applications & Cases Apr. 2018 [Application Note] How to Use ESD/surge Protection Devices : Surge Arresters Surge arresters are GDT (gas discharge tube) voltage protection devices. TDK offers a strong lineup of products with a variety of surge current capabilities ranging from lightning protection for power lines to lightning protection for signal lines. Surge arresters are GDT (gas discharge tube) voltage protection devices. TDK offers a strong lineup of products with a variety of surge current capabilities ranging from lightning protection for power lines to lightning protection for signal lines. Schutzbauelemente Applications & Cases Nov. 2016 [Application Note] Comparison of Chip Capacitors and Chip Varistors in Electrostatic Countermeasures This material describes the characteristics of each protection component, as well as the differences between an MLCC and MLV. This material describes the characteristics of each protection component, as well as the differences between an MLCC and MLV. Schutzbauelemente