Tech Library Products & Technologies (-) Applications & Cases Solution Guides Facet Tech Note List Article Category » Taxonomy term » Name Durchsichtige Leitende Folien EMV-Bauelemente HF-Komponenten Induktivitäten (Spulen) Keramische Schalt- / Heizelemente und Piezo-Komponenten, Schütze, Signaltongeber und Mikrofon Kondensatoren Sensoren und Sensorsysteme Übertrager Facet Tech Note List Product Categories L1 Automobilindustrie ICT Industrie & Energie Medizin & Gesundheitswesen Others Unterhaltungselektronik Wearables Facet Tech Note List Application Category 2022 2021 2020 (-) 2019 2018 2017 2016 2015 2014 Facet Tech Note List Published on Date Applications & Cases Nov. 2019 [Application Note] Motor/Inverter Circuit Configuration Example As the electrification of the automotive progresses, the demand for motor generators is on the rise. There is also a trend towards integration of electric motors and inverters, and the requirements with regard to compact dimensions and resistance against heat and vibrations are becoming ever more severe, while high reliability is also an important factor. In some cases, wiring inductance can lead to high surge voltages which requires countermeasures such as suitable wiring design and snubber capacitors. At the same time, noise countermeasures are also essential. As the electrification of the automotive progresses, the demand for motor generators is on the rise. There is also a trend towards integration of electric motors and inverters, and the requirements with regard to compact dimensions and resistance against heat and vibrations are becoming ever more severe, while high reliability is also an important factor. In some cases, wiring inductance can lead to high surge voltages which requires countermeasures such as suitable wiring design and snubber capacitors. At the same time, noise countermeasures are also essential. Kondensatoren Übertrager Applications & Cases Nov. 2019 [Application Note] Devices that Enhance the Safety of the Digital Cockpit The methods of use of automobiles will change substantially in the future including autonomous driving and car sharing services, and the human machine interface (HMI) between drivers and their cars will also completely change. The methods of use of automobiles will change substantially in the future including autonomous driving and car sharing services, and the human machine interface (HMI) between drivers and their cars will also completely change. Durchsichtige Leitende Folien Keramische Schalt- / Heizelemente und Piezo-Komponenten, Schütze, Signaltongeber und Mikrofon Applications & Cases Nov. 2019 [Application Note] "Vehicle-to-Vehicle and Infrastructure-to-Vehicle Communication" (V2X) to Realize Autonomous Driving Technology The evolution of sensing technology and communication network contribute to the realization of Autonomous driving society and its growth. In association with full-scale expansion of the "5G service" next-generation wireless communication standard, great attention is being placed on wireless technology intended for "vehicle-to-vehicle and infrastructure-to-vehicle communication" (V2X) to communicate data between automobiles and their surroundings. While the TDK Group can offer a lineup of various electronic components for V2X, this article introduces a selection of IMU (Inertial Measurement Unit) and high-frequency products for Telematics Control Units (TCUs). The evolution of sensing technology and communication network contribute to the realization of Autonomous driving society and its growth. In association with full-scale expansion of the "5G service" next-generation wireless communication standard, great attention is being placed on wireless technology intended for "vehicle-to-vehicle and infrastructure-to-vehicle communication" (V2X) to communicate data between automobiles and their surroundings. While the TDK Group can offer a lineup of various electronic components for V2X, this article introduces a selection of IMU (Inertial Measurement Unit) and high-frequency products for Telematics Control Units (TCUs). HF-Komponenten Induktivitäten (Spulen) Sensoren und Sensorsysteme HF-Komponenten Induktivitäten (Spulen) SMD / SMT-Induktivitäten (Spulen) Applications & Cases Juli. 2019 [Application Note] Touch me – feel me! Ob Smartphone, Fahrzeug-Cockpit, Industrie-Steuerung, Haushaltsgerät oder Spielekonsole – piezobasierte Lösungen mit haptischem Feedback gehört die Zukunft. TDK bietet ein einzigartiges Produktportfolio, das sich für alle erdenklichen haptischen Applikationen eignet. Ob Smartphone, Fahrzeug-Cockpit, Industrie-Steuerung, Haushaltsgerät oder Spielekonsole – piezobasierte Lösungen mit haptischem Feedback gehört die Zukunft. TDK bietet ein einzigartiges Produktportfolio, das sich für alle erdenklichen haptischen Applikationen eignet. Sensoren und Sensorsysteme Piezoelectric actuatoren for haptic feedback PowerHap™ Aktuatoren Applications & Cases Juli. 2019 [Application Note] Automotive communication interface: Products recommended for PoC use (PoC filter inductors, chip beads) The demand for high-speed automotive onboard interfaces is increasing, with a view towards supporting driving safety, reducing the environmental load, and improving comfort. For bidirectional communication, the automotive Ethernet format is commonly used, while LVDS is the choice for one-way communication. With LVDS (Low Voltage Differential Signaling), the preferred approach is to also adopt the PoC (Power over Coax) method that enables transmission of the signal and power supply over a single coaxial cable, thereby reducing the weight of wire harnesses in the car. This page describes usage examples and effects of inductors and chip beads specifically recommended for PoC filter applications. The demand for high-speed automotive onboard interfaces is increasing, with a view towards supporting driving safety, reducing the environmental load, and improving comfort. For bidirectional communication, the automotive Ethernet format is commonly used, while LVDS is the choice for one-way communication. With LVDS (Low Voltage Differential Signaling), the preferred approach is to also adopt the PoC (Power over Coax) method that enables transmission of the signal and power supply over a single coaxial cable, thereby reducing the weight of wire harnesses in the car. This page describes usage examples and effects of inductors and chip beads specifically recommended for PoC filter applications. Induktivitäten (Spulen) Induktivitäten (Spulen) SMD / SMT-Induktivitäten (Spulen) Applications & Cases Juni. 2019 [Application Note] Starke Verbindung dank Plasma Um Kunststoffteile sicher zu verkleben, ist eine Oberflächenbehandlung unerlässlich. Eine gleichermaßen einfache wie elegante Lösung ist dabei die Aktivierung mit kaltem Plasma. Relyon Plasma, ein Tochterunternehmen von TDK Electronics, bietet mit dem piezobrush® PZ2 dafür eine handliche Plasmaquelle, die auf dem TDK CeraPlas™ Piezo-Plasmagenerator basiert. Um Kunststoffteile sicher zu verkleben, ist eine Oberflächenbehandlung unerlässlich. Eine gleichermaßen einfache wie elegante Lösung ist dabei die Aktivierung mit kaltem Plasma. Relyon Plasma, ein Tochterunternehmen von TDK Electronics, bietet mit dem piezobrush® PZ2 dafür eine handliche Plasmaquelle, die auf dem TDK CeraPlas™ Piezo-Plasmagenerator basiert. Keramische Schalt- / Heizelemente und Piezo-Komponenten, Schütze, Signaltongeber und Mikrofon Applications & Cases März. 2019 [Application Note] How to Use Power Inductors As electronic devices become more advanced, the power supply voltage of LSIs used in them is lowered, so their power consumption can be reduced and their speed increased. However, a decrease in the power supply voltage also causes the requirements regarding voltage fluctuations to become more severe, creating a need for high-performance DC-DC converters to fulfill these characteristic requirements, and power inductors are important components that greatly affect their performance. TDK has a widely varied lineup of power inductor products, and this article describes and explains effective methods for using power inductors, and key points for selecting them, according to the required characteristics of DC-DC converters. As electronic devices become more advanced, the power supply voltage of LSIs used in them is lowered, so their power consumption can be reduced and their speed increased. However, a decrease in the power supply voltage also causes the requirements regarding voltage fluctuations to become more severe, creating a need for high-performance DC-DC converters to fulfill these characteristic requirements, and power inductors are important components that greatly affect their performance. TDK has a widely varied lineup of power inductor products, and this article describes and explains effective methods for using power inductors, and key points for selecting them, according to the required characteristics of DC-DC converters. Induktivitäten (Spulen) Induktivitäten (Spulen) SMD / SMT-Induktivitäten (Spulen) Applications & Cases März. 2019 [Application Note] Ableitströme drastisch reduzieren und die Anlagenverfügbarkeit erhöhen In drehzahlvariablen Antrieben verursachen die einzelnen Komponenten Ableitströme, die in Summe zum Auslösen des Fehlerstromschutzschalters führen können. Mit dem weiterentwickelten EPCOS LeaXield™ Modul lassen sich diese Ableitströme drastisch reduzieren. In drehzahlvariablen Antrieben verursachen die einzelnen Komponenten Ableitströme, die in Summe zum Auslösen des Fehlerstromschutzschalters führen können. Mit dem weiterentwickelten EPCOS LeaXield™ Modul lassen sich diese Ableitströme drastisch reduzieren. EMV-Bauelemente EMV-Bauelemente Ableitstromfilter LeaXield™