Tech Library Products & Technologies Applications & Cases (-) Solution Guides Facet Tech Note List Article Category » Taxonomy term » Name Drahtlose Energieübertragung EMV-Bauelemente HF-Komponenten Induktivitäten (Spulen) Kondensatoren Schirmungsfolien / Magnetfolien Schutzbauelemente Facet Tech Note List Product Categories L1 (-) Automobilindustrie ICT Industrie & Energie Medizin & Gesundheitswesen Unterhaltungselektronik Wearables Facet Tech Note List Application Category 2021 2020 2019 2018 2017 2016 2015 Facet Tech Note List Published on Date Solution Guides Dez. 2021 [Solution Guide] MLCC Solutions for Power Supply Circuits (Verification of Optimal Structures for Output Capacitors) In the automotive field, CPUs and FPGAs for systems that require advanced image processing, such as onboard ADAS ECUs and autonomous ECUs, need to operate at high speed and require high drive current in conjunction with the increasing performance and functionality of systems. Also, in the ICT field, power supply configurations that support higher current required for devices that need huge amounts of power such as servers. There is a trend towards higher operating speeds and higher currents in the power supply lines of systems with increased performance and functions as described above. At the same time, power supply structures that maintain the nominal voltage within narrow tolerance ranges, which have decreased in conjunction with processor miniaturization, are also required. In the automotive field, CPUs and FPGAs for systems that require advanced image processing, such as onboard ADAS ECUs and autonomous ECUs, need to operate at high speed and require high drive current in conjunction with the increasing performance and functionality of systems. Also, in the ICT field, power supply configurations that support higher current required for devices that need huge amounts of power such as servers. There is a trend towards higher operating speeds and higher currents in the power supply lines of systems with increased performance and functions as described above. At the same time, power supply structures that maintain the nominal voltage within narrow tolerance ranges, which have decreased in conjunction with processor miniaturization, are also required. Kondensatoren Keramik-Vielschichtkondensatoren (MLCC) Solution Guides Nov. 2020 [Solution Guide] Gesamtlösungen für NFC-Schaltungen NFC ist eine Abkürzung für Near Field Communication; es handelt sich um eine Art drahtloser Kommunikation mit kurzer Reichweite. NFC ist eine Funktion, die Datenkommunikation und Authentisierung durchführen kann, wenn zwei NFC-kompatible Geräte in die Nähe zueinander gebracht werden, und ihr Einsatz in Smartphones hat in den letzten Jahren stark zugenommen. Auch in Peripheriegeräten einschließlich tragbarer Endgeräte, wie z.B. Smart-Uhren, ist ein zunehmender Einsatz von NFC zu beobachten. NFC wird in vielen Situationen eingesetzt, u.a. beim bargeldlosen Bezahlen und bei der Authentifizierung von Verbindungen mit Peripheriegeräten, und es wird erwartet, dass es auf dem Weg zu einer berührungslosen Gesellschaft für noch vielfältigere Anwendungen eingesetzt werden wird. Dieser Artikel stellt die wichtigsten Komponenten vor, die in NFC-Schaltungen verwendet werden: NFC-Antenne, Magnetblech, LC-Filterinduktivität, Ein-End-Schaltungsbalun und elektrischer Doppelschichtkondensator (EDLC/Superkondensator). NFC ist eine Abkürzung für Near Field Communication; es handelt sich um eine Art drahtloser Kommunikation mit kurzer Reichweite. NFC ist eine Funktion, die Datenkommunikation und Authentisierung durchführen kann, wenn zwei NFC-kompatible Geräte in die Nähe zueinander gebracht werden, und ihr Einsatz in Smartphones hat in den letzten Jahren stark zugenommen. Auch in Peripheriegeräten einschließlich tragbarer Endgeräte, wie z.B. Smart-Uhren, ist ein zunehmender Einsatz von NFC zu beobachten. NFC wird in vielen Situationen eingesetzt, u.a. beim bargeldlosen Bezahlen und bei der Authentifizierung von Verbindungen mit Peripheriegeräten, und es wird erwartet, dass es auf dem Weg zu einer berührungslosen Gesellschaft für noch vielfältigere Anwendungen eingesetzt werden wird. Dieser Artikel stellt die wichtigsten Komponenten vor, die in NFC-Schaltungen verwendet werden: NFC-Antenne, Magnetblech, LC-Filterinduktivität, Ein-End-Schaltungsbalun und elektrischer Doppelschichtkondensator (EDLC/Superkondensator). Drahtlose Energieübertragung HF-Komponenten Induktivitäten (Spulen) Kondensatoren Schirmungsfolien / Magnetfolien Doppelschichtkondensatoren (EDLC / Supercapacitors) Induktivitäten (Spulen) Drahtlose Energieübertragung / NFC-Antennen (Schild) Solution Guides Dez. 2019 [Solution Guide] Soft Termination Capacitors, Inductors, and Chip Beads for High-Reliability Products for Automotive Applications Automakers are incorporating more multifunctional capabilities into automobiles as they seek to make autonomous driving a reality. Electronic control units (ECUs) for advanced driver assistance systems are consuming more power, and the latest trend is toward ECU integration—installing an ECU close to the engine room or other working part. Automakers are incorporating more multifunctional capabilities into automobiles as they seek to make autonomous driving a reality. Electronic control units (ECUs) for advanced driver assistance systems are consuming more power, and the latest trend is toward ECU integration—installing an ECU close to the engine room or other working part. EMV-Bauelemente Induktivitäten (Spulen) Kondensatoren Induktivitäten (Spulen) SMD / SMT-Induktivitäten (Spulen) Solution Guides Juli. 2019 [Solution Guide] Ensuring communication quality and filtering suitable for PoC (Power over Coax) With the increasing speed and sophistication of interfaces in cars, the PoC (Power over Coax) approach is gaining in popularity, as it allows superimposing signals and power in one coaxial cable, for example for LVDS based automotive camera systems. A PoC filter consisting of one or more inductors and chip beads is used on the circuit side to separate the signal and the power supply current. This is important in terms of maintaining communication quality. The PoC filter therefore requires inductors that realize high impedance for AC components over a wide bandwidth range from low to high frequencies. With the increasing speed and sophistication of interfaces in cars, the PoC (Power over Coax) approach is gaining in popularity, as it allows superimposing signals and power in one coaxial cable, for example for LVDS based automotive camera systems. A PoC filter consisting of one or more inductors and chip beads is used on the circuit side to separate the signal and the power supply current. This is important in terms of maintaining communication quality. The PoC filter therefore requires inductors that realize high impedance for AC components over a wide bandwidth range from low to high frequencies. Induktivitäten (Spulen) Chip Beads SMD / SMT-Induktivitäten (Spulen) Solution Guides Sep. 2018 [Solution Guide] Technical Support Using PI Simulation This is an introduction to our services for technical support which utilize PI simulations to lower the impedance in power-supply lines and reduce the quantity of required decoupling capacitors, by replacing 2-terminal MLCCs with low-ESL capacitors. We hope they will be of use to you in the increasingly severe field of impedance optimized power-supply line design, and in applications for decoupling capacitor compositions and board design techniques, which are continuing to grow in importance. This is an introduction to our services for technical support which utilize PI simulations to lower the impedance in power-supply lines and reduce the quantity of required decoupling capacitors, by replacing 2-terminal MLCCs with low-ESL capacitors. We hope they will be of use to you in the increasingly severe field of impedance optimized power-supply line design, and in applications for decoupling capacitor compositions and board design techniques, which are continuing to grow in importance. Kondensatoren Solution Guides Dez. 2017 [Solution Guide] Vol.3 Application to EV wireless power transfer systems In addition to explaining the characteristics of C0G MLCCs with high withstand voltage, this section focuses on the advantages of replacing the film capacitors used in EV wireless power transfer systems. In addition to explaining the characteristics of C0G MLCCs with high withstand voltage, this section focuses on the advantages of replacing the film capacitors used in EV wireless power transfer systems. Kondensatoren Solution Guides Dez. 2017 [Solution Guide] Vol.2 Application to EV plug-in power charging systems This section mainly explains the advantages of using MLCCs to replace film capacitors in the onboard chargers (OBC) of plug-in charging systems. This section mainly explains the advantages of using MLCCs to replace film capacitors in the onboard chargers (OBC) of plug-in charging systems. Kondensatoren Solution Guides Dez. 2017 [Solution Guide] Vol.1 Features of High voltage MLCCs with C0G Characteristics and Replacement Solutions In recent years, there have been remarkable increases in withstand voltage and capacitance in MLCCs (multilayer ceramic chip capacitors) for temperature compensation (type 1). In particular, even in fields where film capacitors have traditionally been used, resonance circuits for example, replacement with MLCC is now possible. In recent years, there have been remarkable increases in withstand voltage and capacitance in MLCCs (multilayer ceramic chip capacitors) for temperature compensation (type 1). In particular, even in fields where film capacitors have traditionally been used, resonance circuits for example, replacement with MLCC is now possible. Kondensatoren Solution Guides Okt. 2017 [Solution Guide] Measures Against Acoustic Noise in Power Inductors This article introduces some causes of and effective measures against acoustic noise in power inductors, which are main components in power circuits of devices such as DC-DC converters. This article introduces some causes of and effective measures against acoustic noise in power inductors, which are main components in power circuits of devices such as DC-DC converters. Induktivitäten (Spulen) Induktivitäten (Spulen) SMD / SMT-Induktivitäten (Spulen) Solution Guides Mai. 2017 [Solution Guide] Important points regarding mounting 3-terminal feed-through filters The shunt-through connection is a mounting method in which a component is connected in parallel with the power line, and produces an excellent effect for decoupling of the power line. This article will explain each mounting method and their advantages in detail. The shunt-through connection is a mounting method in which a component is connected in parallel with the power line, and produces an excellent effect for decoupling of the power line. This article will explain each mounting method and their advantages in detail. EMV-Bauelemente Seitennummerierung Aktuelle Seite 1 Seite 2 Nächste Seite Next › Letzte Seite Last »