Tech Library Products & Technologies Applications & Cases (-) Solution Guides Facet Tech Note List Article Category » Taxonomy term » Name Drahtlose Energieübertragung EMV-Bauelemente HF-Komponenten Induktivitäten (Spulen) Kondensatoren Schirmungsfolien / Magnetfolien Sensoren und Sensorsysteme Facet Tech Note List Product Categories L1 Automobilindustrie ICT Industrie & Energie Medizin & Gesundheitswesen (-) Unterhaltungselektronik Wearables Facet Tech Note List Application Category 2023 2021 2020 2019 2018 2017 2015 Facet Tech Note List Published on Date Solution Guides März. 2023 [Solution Guide] Solution Guide: Replacing Electrolytic Capacitor with MLCC, Revised Guide Update Traditionally, aluminum electrolytic capacitors and tantalum electrolytic capacitors have been widely used for smoothing and decoupling applications that require large capacitance. With increasing capacitance values, MLCCs are replacing various electrolytic capacitors in power circuits and other applications. Replacing electrolytic capacitors with MLCCs offers various benefits such as space reduction due to smaller size and lower profile, reduced ripple voltage due to low ESR, and improved reliability due to reduced self-heating. On the other hand, low ESR, which is an advantage of MLCCs, can sometimes lead to abnormal oscillation or anti-resonance. Additionally, high dielectric constant MLCCs (Class 2) exhibit a characteristic capacitance change when DC voltage is applied, so caution is necessary. This guide explains the advantages and precautions to be taken when replacing electrolytic capacitors with MLCCs. Traditionally, aluminum electrolytic capacitors and tantalum electrolytic capacitors have been widely used for smoothing and decoupling applications that require large capacitance. With increasing capacitance values, MLCCs are replacing various electrolytic capacitors in power circuits and other applications. Replacing electrolytic capacitors with MLCCs offers various benefits such as space reduction due to smaller size and lower profile, reduced ripple voltage due to low ESR, and improved reliability due to reduced self-heating. On the other hand, low ESR, which is an advantage of MLCCs, can sometimes lead to abnormal oscillation or anti-resonance. Additionally, high dielectric constant MLCCs (Class 2) exhibit a characteristic capacitance change when DC voltage is applied, so caution is necessary. This guide explains the advantages and precautions to be taken when replacing electrolytic capacitors with MLCCs. Kondensatoren Keramik-Vielschichtkondensatoren (MLCC) Solution Guides Sep. 2021 [Solution Guide] Sensors solutions that enable advanced control of service robots Service robots are widely used in various situations such as logistics / transport, security, cleaning, housework, hobbies / entertainment and care / assistance. Since service robots are used in a wide variety of situations, it is necessary to fulfil many requirements such as smooth communication with humans (HMI), ensuring safety and responding to changes in the real time. In service robots, the role of a sensor is very important. In this article, we will take a vacuum cleaner robots as an example. Service robots are widely used in various situations such as logistics / transport, security, cleaning, housework, hobbies / entertainment and care / assistance. Since service robots are used in a wide variety of situations, it is necessary to fulfil many requirements such as smooth communication with humans (HMI), ensuring safety and responding to changes in the real time. In service robots, the role of a sensor is very important. In this article, we will take a vacuum cleaner robots as an example. Sensoren und Sensorsysteme Bewegungssensoren / Inertialsensoren Drucksensoren Temperatursensoren (NTC) Ultraschallsensoren Embedded Motor-Controller IMU (Inertial Measurement Unit) Luftdrucksensoren MEMS-Mikrofone (Mikrofon) NTC-Elemente NTC-Sensor-Systeme SMD-NTC-Thermistoren (Sensoren) Time-of-Flight (ToF) Ultraschallsensoren Solution Guides Nov. 2020 [Solution Guide] Gesamtlösungen für NFC-Schaltungen NFC ist eine Abkürzung für Near Field Communication; es handelt sich um eine Art drahtloser Kommunikation mit kurzer Reichweite. NFC ist eine Funktion, die Datenkommunikation und Authentisierung durchführen kann, wenn zwei NFC-kompatible Geräte in die Nähe zueinander gebracht werden, und ihr Einsatz in Smartphones hat in den letzten Jahren stark zugenommen. Auch in Peripheriegeräten einschließlich tragbarer Endgeräte, wie z.B. Smart-Uhren, ist ein zunehmender Einsatz von NFC zu beobachten. NFC wird in vielen Situationen eingesetzt, u.a. beim bargeldlosen Bezahlen und bei der Authentifizierung von Verbindungen mit Peripheriegeräten, und es wird erwartet, dass es auf dem Weg zu einer berührungslosen Gesellschaft für noch vielfältigere Anwendungen eingesetzt werden wird. Dieser Artikel stellt die wichtigsten Komponenten vor, die in NFC-Schaltungen verwendet werden: NFC-Antenne, Magnetblech, LC-Filterinduktivität, Ein-End-Schaltungsbalun und elektrischer Doppelschichtkondensator (EDLC/Superkondensator). NFC ist eine Abkürzung für Near Field Communication; es handelt sich um eine Art drahtloser Kommunikation mit kurzer Reichweite. NFC ist eine Funktion, die Datenkommunikation und Authentisierung durchführen kann, wenn zwei NFC-kompatible Geräte in die Nähe zueinander gebracht werden, und ihr Einsatz in Smartphones hat in den letzten Jahren stark zugenommen. Auch in Peripheriegeräten einschließlich tragbarer Endgeräte, wie z.B. Smart-Uhren, ist ein zunehmender Einsatz von NFC zu beobachten. NFC wird in vielen Situationen eingesetzt, u.a. beim bargeldlosen Bezahlen und bei der Authentifizierung von Verbindungen mit Peripheriegeräten, und es wird erwartet, dass es auf dem Weg zu einer berührungslosen Gesellschaft für noch vielfältigere Anwendungen eingesetzt werden wird. Dieser Artikel stellt die wichtigsten Komponenten vor, die in NFC-Schaltungen verwendet werden: NFC-Antenne, Magnetblech, LC-Filterinduktivität, Ein-End-Schaltungsbalun und elektrischer Doppelschichtkondensator (EDLC/Superkondensator). Drahtlose Energieübertragung HF-Komponenten Induktivitäten (Spulen) Kondensatoren Schirmungsfolien / Magnetfolien Doppelschichtkondensatoren (EDLC / Supercapacitors) Induktivitäten (Spulen) Drahtlose Energieübertragung / NFC-Antennen (Schild) Solution Guides Jan. 2019 [Solution Guide] TDMA Noise Countermeasures, Reception Sensitivity Improvement, and ESD (Electrostatic Discharge) Countermeasures in Microphone Lines, Using Noise Suppression Filters and ESD Notch Filters If communication waves from cellular or Wi-Fi sources interfere with and intrude into microphone lines for smartphones or other devices, some of their components will become noise components in audible bands known as "TDMA noise", and may be emitted from speakers as unpleasant sound. Countermeasures which implement combinations of TDK's noise suppression filters and ESD Notch Filters can not only demonstrate outstanding effectiveness at suppressing TDMA noise with no effect on signals, but can also provide a variety of other benefits such as improving cellular or Wi-Fi communication reception sensitivity, and providing countermeasures against ESD (electrostatic discharge). If communication waves from cellular or Wi-Fi sources interfere with and intrude into microphone lines for smartphones or other devices, some of their components will become noise components in audible bands known as "TDMA noise", and may be emitted from speakers as unpleasant sound. Countermeasures which implement combinations of TDK's noise suppression filters and ESD Notch Filters can not only demonstrate outstanding effectiveness at suppressing TDMA noise with no effect on signals, but can also provide a variety of other benefits such as improving cellular or Wi-Fi communication reception sensitivity, and providing countermeasures against ESD (electrostatic discharge). EMV-Bauelemente Entstörfilter Kerbfilter mit ESD-Schutzfunktion Solution Guides Sep. 2018 [Solution Guide] Technical Support Using PI Simulation This is an introduction to our services for technical support which utilize PI simulations to lower the impedance in power-supply lines and reduce the quantity of required decoupling capacitors, by replacing 2-terminal MLCCs with low-ESL capacitors. We hope they will be of use to you in the increasingly severe field of impedance optimized power-supply line design, and in applications for decoupling capacitor compositions and board design techniques, which are continuing to grow in importance. This is an introduction to our services for technical support which utilize PI simulations to lower the impedance in power-supply lines and reduce the quantity of required decoupling capacitors, by replacing 2-terminal MLCCs with low-ESL capacitors. We hope they will be of use to you in the increasingly severe field of impedance optimized power-supply line design, and in applications for decoupling capacitor compositions and board design techniques, which are continuing to grow in importance. Kondensatoren Solution Guides Dez. 2017 [Solution Guide] Vol.1 Features of High voltage MLCCs with C0G Characteristics and Replacement Solutions In recent years, there have been remarkable increases in withstand voltage and capacitance in MLCCs (multilayer ceramic chip capacitors) for temperature compensation (type 1). In particular, even in fields where film capacitors have traditionally been used, resonance circuits for example, replacement with MLCC is now possible. In recent years, there have been remarkable increases in withstand voltage and capacitance in MLCCs (multilayer ceramic chip capacitors) for temperature compensation (type 1). In particular, even in fields where film capacitors have traditionally been used, resonance circuits for example, replacement with MLCC is now possible. Kondensatoren Solution Guides Okt. 2017 [Solution Guide] Measures Against Acoustic Noise in Power Inductors This article introduces some causes of and effective measures against acoustic noise in power inductors, which are main components in power circuits of devices such as DC-DC converters. This article introduces some causes of and effective measures against acoustic noise in power inductors, which are main components in power circuits of devices such as DC-DC converters. Induktivitäten (Spulen) Induktivitäten (Spulen) SMD / SMT-Induktivitäten (Spulen) Solution Guides Febr. 2015 [Solution Guide] Flex Crack Countermeasures in MLCCs TDK offers special types of MLCC products with redundancy design, in order to avoid short circuit failures and improve the reliability of equipment. Please select products that suit your purposes and use them to improve the reliability of your products. TDK offers special types of MLCC products with redundancy design, in order to avoid short circuit failures and improve the reliability of equipment. Please select products that suit your purposes and use them to improve the reliability of your products. Kondensatoren Solution Guides Febr. 2015 [Solution Guide] Solder Crack Countermeasures in MLCCs This atricle introduces major causes and countermeasures of solder crack in MLCCs (Multilayer Ceramic Chip Capacitors). This atricle introduces major causes and countermeasures of solder crack in MLCCs (Multilayer Ceramic Chip Capacitors). Kondensatoren