FAQ
Q.
Please explain how to interpret the output power when the set voltage is used after being lowered below the rated output voltage.
  • Power Supplies
  • >
  • DC-DC Converters
  • /
  • AC-DC Power Supplies


A. The maximum output current that can be used increases if the set voltage is lowered when “maximum output power = rated output voltage × maximum output current” is used, but please use at the specified values of the maximum output current or below because there is the danger of damage due to factors such as the generation of heat in the components inside the power supply.