Tech Library Products & Technologies Applications & Cases Solution Guides Facet Tech Note List Article Category » Taxonomy term » Name Capacitors Ceramic Switching / Heating, Piezo Components, Contactors, Buzzers and Microphones EMC Components Ferrites and Accessories Inductors (Coils) Noise Suppressing / Magnetic Sheets Sensors and Sensor Systems Transformers Transparent Conductive Film (-) Voltage / Current / Temperature Protection Devices Wireless Power Transfer Facet Tech Note List Product Categories L1 Automotive Consumer Electronics ICT Industrial & Energy (-) Medical & Healthcare Others Wearables Facet Tech Note List Application Category 2020 2018 2017 2016 Facet Tech Note List Published on Date Products & Technologies Apr. 2020 [Product Overview] What is the difference between Zener/TVS diodes and varistors? Four comparison aspects to consider with regard to usage Chip varistors and TVS diodes are commonly used as over-voltage protection components. Their structural design and manufacturing methods are completely different, but they offer similar characteristics with regard to protection from static electricity. They generally can therefore be used interchangeably in a circuit, but there are cases where chip varistors are considered to be not suitable. For historical reasons, many of the specification items given in catalogs and data sheets are different, which makes it difficult to compare characteristics based solely on these data, unlike in the case of capacitors and other general components. The aim of this article is to clarify the difference between varistors and diodes and to introduce data that can be used to compare the two. Chip varistors and TVS diodes are commonly used as over-voltage protection components. Their structural design and manufacturing methods are completely different, but they offer similar characteristics with regard to protection from static electricity. They generally can therefore be used interchangeably in a circuit, but there are cases where chip varistors are considered to be not suitable. For historical reasons, many of the specification items given in catalogs and data sheets are different, which makes it difficult to compare characteristics based solely on these data, unlike in the case of capacitors and other general components. The aim of this article is to clarify the difference between varistors and diodes and to introduce data that can be used to compare the two. Voltage / Current / Temperature Protection Devices Voltage Protection Devices Chip Varistors / Ceramic Transient Voltage Suppressors Applications & Cases Oct. 2018 [Application Note] Combined current control High-power loads are a major stress factor when fuses and components are switched on, as they cause very high currents to flow. To avoid this, TDK offers ceramic EPCOS inrush current limiters, based on NTC and PTC thermistors – a strong duo when used in combination. High-power loads are a major stress factor when fuses and components are switched on, as they cause very high currents to flow. To avoid this, TDK offers ceramic EPCOS inrush current limiters, based on NTC and PTC thermistors – a strong duo when used in combination. Voltage / Current / Temperature Protection Devices PTC Inrush Current Limiters Products & Technologies Oct. 2018 [Product Overview] Compact overvoltage protection with an integrated fuse TDK Corporation (TSE:6762) has extended its EPCOS ThermoFuse™ family of fuse protected varistors with the new compact NT14 and NT20 series. The new ThermoFuse components feature a footprint that fits into existing circuit board layouts. TDK Corporation (TSE:6762) has extended its EPCOS ThermoFuse™ family of fuse protected varistors with the new compact NT14 and NT20 series. The new ThermoFuse components feature a footprint that fits into existing circuit board layouts. Voltage / Current / Temperature Protection Devices Voltage Protection Devices ThermoFuse Varistors Applications & Cases May. 2018 [Application Note] How to Use ESD/surge Protection Devices : SMD Varistors SMD or chip varistors are voltage-dependent resistors based on ceramic multilayer technology. They are widely used to protect electronic circuits in consumer devices and telecom, industrial and automotive applications against transient overvoltages, such as electrostatic discharges (ESD) and surge transients. SMD or chip varistors are voltage-dependent resistors based on ceramic multilayer technology. They are widely used to protect electronic circuits in consumer devices and telecom, industrial and automotive applications against transient overvoltages, such as electrostatic discharges (ESD) and surge transients. Voltage / Current / Temperature Protection Devices Voltage Protection Devices Chip Varistors / Ceramic Transient Voltage Suppressors Applications & Cases May. 2018 [Application Note] The Optimal Applications for Chip Varistors for ESD Countermeasures Chip varistors have both surge absorption capabilities and noise suppressing effects. See the adaptive application fields of various components for ESD countermeasures as well as the optimal application fields of TDK’s chip varistors / ceramic transient voltage suppressors, CeraDiodes, and multilayer chip protectors. Chip varistors have both surge absorption capabilities and noise suppressing effects. See the adaptive application fields of various components for ESD countermeasures as well as the optimal application fields of TDK’s chip varistors / ceramic transient voltage suppressors, CeraDiodes, and multilayer chip protectors. Voltage / Current / Temperature Protection Devices Voltage Protection Devices Chip Varistors / Ceramic Transient Voltage Suppressors Applications & Cases Apr. 2018 [Application Note] Chip Varistors Prevent Damage of Electronics from Electrostatic Discharge TDK’s chip varistors in the AVR series, which are made with our own materials, feature high resistance to repeated surges. Products that substitute Zener diodes in compact devices such as solenoid valves and stepping motors, which are rapidly and frequently turned on and off, are also available. TDK’s chip varistors in the AVR series, which are made with our own materials, feature high resistance to repeated surges. Products that substitute Zener diodes in compact devices such as solenoid valves and stepping motors, which are rapidly and frequently turned on and off, are also available. Voltage / Current / Temperature Protection Devices Voltage Protection Devices Chip Varistors / Ceramic Transient Voltage Suppressors Applications & Cases Apr. 2018 [Application Note] How to Use Temperature Protection Devices : Chip NTC Thermistors NTC thermistors are heat-sensitive resistor elements of which resistance values rapidly decrease with rise of temperature. With this property, they are used as temperature protection devices for protecting circuits from overheating as well as temperature sensors. TDK offers various sizes of both TDK brand and EPCOS brand SMD NTC thermistors by capitalizing on our accumulated material technologies and a multilayer processing technology. This article describes temperature protection device applications for temperature detection and temperature compensation. NTC thermistors are heat-sensitive resistor elements of which resistance values rapidly decrease with rise of temperature. With this property, they are used as temperature protection devices for protecting circuits from overheating as well as temperature sensors. TDK offers various sizes of both TDK brand and EPCOS brand SMD NTC thermistors by capitalizing on our accumulated material technologies and a multilayer processing technology. This article describes temperature protection device applications for temperature detection and temperature compensation. Voltage / Current / Temperature Protection Devices Temperature Protection Devices Chip NTC Thermistors (Protection Device) Applications & Cases Apr. 2018 [Application Note] Circuit Protection Devices / Voltage Protection Devices Surge arresters are GDT (gas discharge tube) voltage protection devices. TDK offers a strong lineup of products with a variety of surge current capabilities ranging from lightning protection for power lines to lightning protection for signal lines. Surge arresters are GDT (gas discharge tube) voltage protection devices. TDK offers a strong lineup of products with a variety of surge current capabilities ranging from lightning protection for power lines to lightning protection for signal lines. Voltage / Current / Temperature Protection Devices Voltage Protection Devices Surge Arresters Solution Guides Mar. 2017 [Solution Guide] Audio line solution guide for smartphones using chip varistors TDK’s chip varistors are ESD protection components that can solve various needs that are specific to audio lines. We shall now explain the various advantages providing the optimal solutions for the audio lines of smartphones. TDK’s chip varistors are ESD protection components that can solve various needs that are specific to audio lines. We shall now explain the various advantages providing the optimal solutions for the audio lines of smartphones. Voltage / Current / Temperature Protection Devices Voltage Protection Devices Chip Varistors / Ceramic Transient Voltage Suppressors Applications & Cases Nov. 2016 [Application Note] Comparison of Chip Capacitors and Chip Varistors in Electrostatic Countermeasures This material describes the characteristics of each protection component, as well as the differences between an MLCC and MLV. This material describes the characteristics of each protection component, as well as the differences between an MLCC and MLV. Voltage / Current / Temperature Protection Devices Voltage Protection Devices Chip Varistors / Ceramic Transient Voltage Suppressors