Contact

FAQ

Q.Why is inductance specified by numbers such as 1, 1.5, 2.2, 3.3, etc.?

Inductors (Coils) >  Inductors (Coils) >  Inductors (Coils)

A. This is because inductance is based on the preferred number series for passive components taking tolerances into consideration, as prescribed in JIS C 5063.
For inductors, E6 (tolerance: 20%), E12 (10%), E24 (5%) series are often used, and in the E6 series, for example, inductance is specified as 1, 1.5, 2.2, 3.3, 4.7, 6.8, 10, 15, etc.

 

Has this FAQ been useful? YesNo

All related FAQ