Contact

FAQ

Q.Would it be a problem to use inductors in parallel?

Inductors (Coils) >  Inductors (Coils) >  Inductors (Coils)

A. It is possible to use inductors in parallel.
When inductors are used in parallel, a greater amount of current can flow.
However, there is the disadvantage that inductance will decrease, as it is a synthetic inductance.
The synthetic inductance Lt can be obtained using the following formula:

Has this FAQ been useful? YesNo

All related FAQ