Contact

FAQ

Q.Would it be a problem to use chip beads in parallel?

EMC Components >  EMC Components >  Chip Beads

A. It is possible to use chip beads in parallel.
When chip beads are used in parallel, a greater amount of current can flow.
However, there is the disadvantage that impedance value will decrease, as it is a synthetic impedance.
The synthetic impedance Zt can be obtained using the following formula:

Has this FAQ been useful? YesNo

All related FAQ