Contact

FAQ

Q.What is the zero load resistance value?

Voltage / Current / Temperature Protection Devices/ Sensors and Sensor Systems >  Temperature Protection Devices/ Temperature Sensors (NTC) >  Chip NTC Thermistors (Protection Device)/ Chip NTC Thermistors (Sensor)

A. Resistance value of a thermistor measured at a prescribed temperature, also called no-load resistance value.
The value is normally measured at a standard temperature of 25°C.
The measurement is conducted at a power level such that the influences of spontaneous heat generation can be negligible.

Has this FAQ been useful? YesNo

All related FAQ