Contact

FAQ

Q.What is the B constant?

Voltage / Current / Temperature Protection Devices/ Sensors and Sensor Systems >  Temperature Protection Devices/ Temperature Sensors (NTC) >  Chip NTC Thermistors (Protection Device)/ Chip NTC Thermistors (Sensor)

A. A constant representing change in resistance, calculated using the resistance value at two specified ambient temperatures according to the following formula.

B=ln (R/R0) / (1/T-1/T0)

R: Resistance value at time when ambient temperature is T (K) R0: Resistance value at time when ambient temperature is T0 (K)

Has this FAQ been useful? YesNo

All related FAQ