Contact

FAQ

Q.What is withstand voltage?

Voltage / Current / Temperature Protection Devices/ Sensors and Sensor Systems >  Temperature Protection Devices/ Temperature Sensors (NTC) >  Chip NTC Thermistors (Protection Device)/ Chip NTC Thermistors (Sensor)

A. Indicates the amount of voltage that can be resisted when applied for three minutes in still air at 25°C. Withstand voltage is measured using a method that starts at 0V and then gradually increases the amount of voltage applied.

Has this FAQ been useful? YesNo

All related FAQ