Contact

FAQ

Q.What is discharge voltage?

Voltage / Current / Temperature Protection Devices >  Voltage Protection Devices >  Chip Varistors / Ceramic Transient Voltage Suppressors

A. The peak value of the voltage between varistor terminals when a specified standard surge current is applied. It is also known as the "clamping voltage", and is generally measured using a 8/20us lightning surge test waveform.

Has this FAQ been useful? YesNo

All related FAQ