Contact

FAQ

Q.Can the capacitors (Multilayer Capacitors with Leads) be used with AC voltages at commercial frequencies?

Capacitors >  Ceramic Capacitors >  MLCC with Dipped Radial Lead

A. Voltages that can be applied to the capacitors need to be designed so that the peak to peak voltage does not exceed the rated voltage. In the case of voltage that is superimposed on an DC voltage, the peak voltage must be designed not to exceed the rated voltage. In addition, in cases where resonances or surge voltages are transitionally applied, these abnormal voltages must not exceed the rated voltage as well.


>>MLCC with Dipped Radial Lead

For any other product-related questions or inquiries, please contact us throughone of our sales representatives or this website.

Has this FAQ been useful? YesNo