Contact

FAQ

Q.Can the capacitors (Multilayer Capacitors with Leads) be used with their leads bent?

Capacitors >  Ceramic Capacitors >  MLCC with Dipped Radial Lead

A. They can be used with their leads bent as long as no mechanical stress is applied to the capacitor main unit when the leads are bent. If breakage or cracking occurs on the resin of the capacitors, do not use them.

Figure 1

When bending the lead wires, fix the lead wires on the capacitor main unit side at the bent locations as shown in Figure 1, so as to avoid impacts to the capacitor main unit.


>>MLCC with Dipped Radial Lead

For any other product-related questions or inquiries, please contact us throughone of our sales representatives or this website.

Has this FAQ been useful? YesNo