Contact

FAQ

Q.What is the proper way to select an appropriate filter for inverters?

EMC Components >  EMC Components >  Power Line EMC Filters

A. Select a filter based on the safety standards and noise level required for the device in which the filter is to be used, and based on the power supply to be used. The models for which the expression “for use with inverters” is indicated in the selection chart are the main ones to be selected. In general, selection of a filter with superior attenuation characteristics for 150 to 500kHz or so is appropriate.

Has this FAQ been useful? YesNo

All related FAQ