Contact

FAQ

Q.Can power modules / on-board power supplies be operated just by connecting input-output terminals to power supplies and load devices?

Power Supplies >  Switching Power Supply >  AC-DC Power Supplies/ DC-DC Converters

A. There are power supplies that cannot be operated just by connecting input-output terminals to power supplies and load devices. Please be sure to note the following precautions.
- Products with sensing functions require the sensing terminals to be connected with the output sides.
- Products with remote ON/OFF control functions sometimes require connections with the -Vin terminals or +Vin terminals.
- Some products require peripheral components such as capacitors or choke coils.
Refer to the instruction manuals and basic connections of the respective products for details.

Has this FAQ been useful? YesNo