Contact

FAQ

Q.The catalog says “operating temperature: –30 to +105°C” and gives a storage temperature that is lower stating “storage temperature: –30 to +85°C”, but isn’t it the opposite?

Ferrites and Accessories >  Ferrites and Accessories >  Ferrite Cores

A. The storage temperature in the catalog is stated on the premise that the product is in its package so there is the concern of a malfunction if it is stored at over +85°C.
+105°C is fine with single ferrite body.

Has this FAQ been useful? YesNo