联系我们

常见问题

Q.Why should I use these technical support tools?

电容器/ 电感器(线圈)/ EMC对策产品/ RF产品和模块/ 电压/电流/过热保护器件/ 变压器 >  陶瓷电容器/ 电感器(线圈)/ EMC对策产品/ RF产品和模块/ 电压保护器件/ 变压器 >  积层贴片陶瓷片式电容器/ 三端子贯通型MLCC/ 电感器(线圈)/ 片式磁珠/ 3端子滤波器/ 共模滤波器/扼流圈/ 噪音滤波器/ 平衡器/ 贴片压敏电阻/陶瓷瞬时电压抑制器/ LAN用脉冲变压器和模块

A. Recently, electrical circuits designs use simulation technology. In order to improve simulation accuracy, it is very important to acquire a simulation model that is as close as possible to the actual usage. For example, when a 1uF capacitor is used, ESR (Equivalent Series Resistance) and ESL (Equivalent Series Inductance) differ depending on the size. Therefore, if you create a circuit using the ideal capacitor determined by simulation, actual results may be very different. By using a simulation model, you can attain results that are as close as possible to actual phenomena.

该FAQ是否对你有所帮助? 有帮助没有帮助