Attracting Tomorrow TDK

TDK Prototype Biomagnetic Sensor: PotentialAlternative to SQUID (Superconducting Quantum Interference Device)
Designed to Detect Extremely Weak Biomagnetic Signals at Room Temperature
The World’s First Ambient Temperature Sensor to Visualize the Heart’s Magnetic Field Distribution

Video Player is loading.
Current Time 0:00
Duration 0:00
Loaded: 0%
Stream Type LIVE
Remaining Time 0:00
 
1x
    • Chapters
    • descriptions off, selected
    • captions off, selected
    • en (Main), selected

    Sensors are one of TDK’s key technologies. We are focused on development of a wide variety of sensors for various applications. One of these is a prototype magnetic sensor designed to measure very weak biomagnetic fields. This technology is being developed to open up the possibility of finding solutions to problems, such as the existence of heart disease in an unborn infant, which cannot be discovered using an existing electrocardiograph, or ischemic heart disease which is difficult to detect at an early stage.

    TDK has developed compact prototype biomagnetic sensors through development of applications with MR (magnetoresistive) element technology utilizing spintronics technology that was cultivated through the manufacture of HDD (hard disc drive) heads. These prototype sensors are designed to make it possible to sense weak biomagnetic fields which currently can only be measured by using a SQUID (Superconducting Quantum Interference Device) flux meter. And, through collaborative research with the graduate school of the Tokyo Medical and Dental University, TDK has developed a prototype biomagnetic measurement system using a multi-channel sensor array, and we are the first in the world to successfully carry out proof-of-concept measurement and visualization (imaging) of the cardiac magnetic fields using MR sensors. Unlike the SQUID flux meter, which is an expensive and bulky system that also requires a cooling device using liquid helium (Dewar), this prototype system, which uses MR sensors, is being developed for measurement with high sensitivity even at room temperature. It is also designed to be compact and to provide excellent operability and portability. As a result, it is expected to have applications not only in the field of medical diagnosis such as magnetocardiography, but also in the fields of health care and sports science.

    Design features of the prototype MR biomagnetic sensors from TDK

    • Compact and biomagnetic sensors using MR elements with spintronics technology
    • Being developed for a magnetic resolution with an order of magnitude in the tens of pT (10-11T), which is close to the SQUID domain.
    • Designed to be used to non-invasively measure biomagnetic fields such as the cardiac magnetic fields, and muscle magnetic fields, at room temperature.
    • A sensor array with multiple channels is designed to visualize the magnetic field distribution of the heart.
    • Does not require a cooling system.
    • Designed for portability.
    • Collaborative research with the graduate school of the Tokyo Medical and Dental University
    • World’s first success about magneto-cardiometry under regular conditions (outside a magnetically shielded room) by Tokyo Medical and Dental University in 2024.

    Background

    Heart disease, along with cancer (malignant growth) and cerebrovascular disease (cerebral hemorrhage), is the leading cause of death worldwide.
    The electrocardiograph is widely used as a diagnostic device to determine the status of cardiac activity.

    The source of electrical activity of the heart is a bundle of cells known as the sinus node, which is a natural pacemaker located in the right atrium. The electrical signals produced by the sinus node are first conveyed to the entire atrium, and then pass through the tissue known as the atrioventricular node, after which they branch to the right and left, and are conveyed to the entire ventricle, causing the rhythmic repetitive beating of the heart. This is known as the impulse conduction system. This conduction of the electrical excitation of the heart appears as the potential difference between different parts on the surface of the body. The electrocardiograph detects and amplifies this potential difference using multiple electrodes attached to the extremities as well as the chest, and displays and records it as waveforms.

    Figure 1 shows the cardiac impulse conduction system, general flow of cardiac activity current, and the pattern diagram of a typical electrocardiogram waveform. P-wave and QRS-wave are waveforms which accompany the contraction of the atrium and ventricles respectively, while T-wave and U-wave are waveforms of the processes by which the excitation of ventricles are cooling down.

    Figure 1 Cardiac impulse conduction system and electrocardiogram waveform

    Figure 1 Cardiac impulse conduction system and electrocardiogram waveform

    If we were able to observe the detailed working of the cardiac muscles, it could result in a remarkable improvement in the accuracy of diagnosis. The magnetocardiograph (MCG) is being developed and tested to address these problems. According to the “right-hand screw rule” in electromagnetism, when current flows, it produces magnetic fields around it. Hence, by measuring the magnetic fields produced around the heart, it is theoretically possible to estimate the flow of current, and the parts to which it flows. Another anticipated advantage of the magnetocardiograph is that it is designed to carry out measurement completely non-invasively while the subject is fully clothed, and would not require electrodes to be attached to the surface of the body. But, cardiac magnetic fields are extremely weak biomagnetic fields, and hence the magnetocardiograph will need to be equipped with highly sensitive magnetic sensors.

    Types of Magnetic Sensors and Biomagnetic Fields

    The first electrocardiogram was measured in 1903 using a device invented by W.
    Einthoven, a Dutch physicist. In comparison with this, cardiac magnetic fields are extremely weak at about 1 millionth or less of geomagnetism, and hence they were fist measured only in the latter half of the 20th century, in the year 1963. The first measurement used a pair of magnetic flux detection coils wound as many as 2 million times. After this, measurement was carried out in a special magnetically shielded room, in order to prevent disturbance from geomagnetism, but even then, it was barely enough to determine that magnetic fields were being produced by the heart, and the accuracy was not enough to be useful in diagnosis of heart disease.
    The SQUID flux meter developed around 1970 has brought about major advances in the measurement of biomagnetic fields. SQUID is the acronym for “superconducting quantum interference device”, and it is a magnetic sensor in which a Josephson junction is created in a part of the coil using a superconductor. The Josephson junction element was originally developed as a logic element to increase the computer processing speed, but since it is extremely sensitive to magnetism, it was used as a highly sensitive flux meter. Using this SQUID flux meter, it has become possible to measure not only the magnetic fields which accompany cardiac activity, but also to measure brain magnetic fields.

    However, to operate SQUID, it is necessary to cool the superconductive coil using liquid helium, and to set up a special magnetically shielded room to block magnetic noise, as a result of which the system becomes bulky and expensive. This is the reason why biomagnetic field measurement devices using a SQUID flux meter are used to a very limited extent,. For example, there are only about 40 devices in Japan, and most of them are used for magnetoencephalograms and only 2 devices are for magnetocardiograms (in 2020).
    Several papers have pointed out that analyzing an electrocardiogram by comparing it with a magnetocardiogram can be useful in the diagnosis of various heart diseases. However, in practical terms, an extremely highly sensitive magnetic sensor that can replace the SQUID flux meter is likely to better promote the development and spread of the magnetocardiograph. TDK has is working on developing new biomagnetic sensors using advanced MR (magnetoresistive) elements, which are anticipated to achieve a magnetic resolution in the SQUID domain. Currently research is continuing with the goal of reaching a just a several pT. However, additional testing and development is required.

    The sensitivity (approximate measurement range) and biomagnetic field intensity of various magnetic sensors that have been actually developed are summarized in Figure 4. The unit of magnetic field intensity is [Wb/m], and the unit of magnetic flux density is [Wb/m2]. Both are related through magnetic permeability, but the magnetic permeability of biological tissue, which is non-magnetic material, is approximately 1, which is the same as air, and hence, in this figure, the intensity of the magnetic field is represented by the magnetic flux density. 1Wb/m2 = 1T (Tesla). 1T is equal to 104G (Gauss) in the cgs unit system.

    Figure 2 Approximate range of measurement of various magnetic sensors

    Figure 2 Approximate range of measurement of various magnetic sensors

    Development of HDD Head Technology and MR Elements

    We shall briefly describe the MR elements used in the prototype biomagnetic sensors from TDK.
    We have known for a long time that when an external magnetic field is applied on a substance, the electrical resistance changes slightly, and this is known as the magnetoresistive effect (MR effect). This type of physical effect, along with the Hall effect, is collectively known as the “galvanomagnetic effect”. When electrons and electron holes carrying electric charge move inside a magnetic field, the Lorentz force acts, causing the direction of movement to bend. MR sensors use the magnetoresistive effect of semiconductors and ferromagnetic materials, and are being widely used as magnetic sensors to detect magnetic data on tickets at automated ticket gates, magnetic ink patterns on banknotes, etc.

    Other than the conventional type of magnetoresistive effect, a multi-layered film made of ferromagnetic materials demonstrates a magnetoresistive effect with an abnormally large rate of change of resistance. In 1987, P. Grunberg and A. Fert discovered this phenomenon known as the giant magnetoresistive effect. It cannot be explained by the galvanomagnetic effect, and it is a spintronics phenomenon that is related to the spin of electrons.
    The giant magnetoresistive effect is used as the reading element in an HDD, and since the latter half of the 1990s, it has resulted in rapid growth of recording density in HDDs. TDK has quickly adopted advanced spintronics technology, and has developed HDD heads such as the GMR head and TMR head in quick succession, and we have been contributing to the capacity enlargement of HDDs. (Figure 3).

    Figure 3 Phases of magnetic head development by TDK and increasing recording density of HDDs

    Figure 3 Phases of magnetic head development by TDK and increasing recording density of HDDs

    This article presents prototype biomagnetic sensors, which are designed to use MR magnetic sensors of the spintronics type, developed by application of thin-film technology, cultivated through the manufacture of HDD heads. So far, even the spintronics type MR magnetic sensors had a limit on sensitivity equal to 10nT (10-8T), and to enable measurement of magnetic field gradients on the order of a few pT, which is considered impossible with MR elements, a technology that largely increases signal-to-noise ratio as a sensor is required.

    By eliminating environmental noises including one of earth magnetism, which is a million times as intense as noise of biomagnetic fields, and noises of MR elements and circuits themselves, TDK is working to develop biomagnetic sensors with a very high magnetic resolution of a few tens of pT (10-11T), which is about 1000 times higher than before. This would be close to the domain of the SQUID flux meter, and it also may be developed to enable measurement of biomagnetic fields such as cardiac magnetic fields.

    Principle of the Spintronics Type MR Magnetic Sensor

    The spintronics type MR element has a sandwich structure made of a thin-film of non-magnetic material sandwiched between thin ferromagnetic films. One of the ferromagnetic films is a pin layer (fixed layer) in which the direction of magnetization is fixed by pinning, and the other ferromagnetic film is a free layer in which the direction of magnetization follows the direction of the external magnetic field. Since the electrical resistance of the element varies proportionately with the relative angle between the direction of magnetization of the pin layer and free layer, the intensity of the magnetic field can be measured from the magnitude of the current.

    Figure 4:Basic structure and sensor principle of the MR element

    Figure 4 Basic structure and sensor principle of the MR element

    Unlike fluxgate sensors and MI (Magneto-Impedance) sensors, MR magnetic sensors receive signals just by applying DC power source, and do not require complex oscillation circuits.

    An MR element also has excellent temperature characteristics, and the resistance value changes only slightly due to changes in temperature. In order to minimize this temperature drift, multiple elements are formed on the circuit board of the MR magnetic sensor, and a bridge configuration is used for differential temperature compensation. An ordinary Wheatstone bridge circuit in which 4 elements have been combined is shown in Figure 5. The arrows indicate the direction of magnetization of the pin layer.

    Figure 5:Example of the bridge configuration for temperature compensation (Wheatstone bridge)

    Figure 5 Example of the bridge configuration for temperature compensation (Wheatstone bridge)

    Development and Testing of Prototype Biomagnetic Sensors for Visualization (Imaging) of the Magnetic Fields of the Heart for the First Time

    The MR magnetic sensor unit combines multiple MR elements in a bridge configuration, and has a built-in low-noise circuit. TDK has developed a prototype sensor array in which these sensor units are arranged in the form of a lattice, and through collaborative research with the graduate school of the Tokyo Medical and Dental University, we have become the first organization in the world to successfully carry out proof-of-concept measurement and visualization (imaging) of the cardiac magnetic fields using MR magnetic sensors (in 2016).
    TDK has continued to optimize the design by increasing the number of channels up to 64 to obtain clearer images. Figure 6 shows a prototype MR magnetic sensor unit from TDK and a 64ch (channel) sensor array.

    Figure 6 Image showing the MR magnetic sensor unit (upper left) and a 64ch MR magnetic sensor array

    Figure 6 Image showing the MR magnetic sensor unit (upper left) and a 64ch MR magnetic sensor array

    Figure 7 shows an example from proof-of-concept testing of measurement and visualization of cardiac magnetic field distribution using TDK's 64ch MR magnetic sensor arrays. The blue waveform is an electrocardiogram (ECG), the green waveform is a magnetocardiogram (MCG), and the picture is the magnetic field distribution of the heart superimposed on the X-ray image of the chest. The black dots are sensor channels and the waveform of the magnetocardiogram is the time waveform of magnetic field intensity obtained from sensor channels indicated by yellow dots (①and②). The peak of one of the waveforms faces the opposite direction of the other one because of the difference in direction of the lines of magnetic force.
    The white curved lines in the photo, which are similar to the isobar lines of a weather map, connect points with magnetic field intensity equal to around the heart at the time of measurement supporting R waves of the electrocardiogram. The red area and blue area represent the differences in the direction of the lines of magnetic force. The red area shows the direction in which the line of magnetic force is ballooning. The blue area shows the direction in which the line of magnetic force is drawing inwards. R waves of the electrocardiogram accompany the contraction of the ventricles. Judging from the magnetic field distribution, direction of the line of magnetic force, and the right hand screw rule, it can be estimated that the action potential of the heart at this time is flowing in the direction shown by the green arrow.

    Figure 7

    Figure 7 Example from proof-of-concept testing of measurement and visualization of cardiac magnetic field distribution using a 64ch MR magnetic sensor array

    Future Potential Benefits of Magnetocardiograph

    The prototype biomagnetic measurement system being developed by TDK, which uses MR elements is being designed to be a more convenient and less expensive system than the SQUID flux meter, which is expensive, bulky, and requires a liquid helium cooling device (Dewar). In addition, TDK’s new biomagnetic system is being developed to enable measurement at room temperature (without cooling), and to allow for improved operability and portability.
    Additionally, the new system is being developed for use with, a relatively simple shielded room. MR sensors have a wider dynamic range than SQUID, and hence it is anticipated that they work even with simple magnetic shielding. TDK is demonstrating, through proof-of-concept, that measurement of the cardiac magnetic field distribution is actually possible inside our unprecedentedly innovative portable compact magnetic shield. In addition, Tokyo Medical and Dental University is the first in the world to realize successful magneto-cardiometry under regular conditions (outside a magnetically shielded room) in 2024.TDK's prototype sensors require neither cooling nor a Dewar, the arrangement and density of sensors is designed to be changed freely depending on target parts.

    The application of magnetocardiograms for clinical diagnosis is still in the initial development phase, and once magnetocardiographs, which can be used at room temperature, are fully developed, tested, and cleared or approved by the relevant regulatory authorities, they may usher in major innovations in the diagnosis of heart diseases as well as other diseases.
    For example, the images obtained as X-ray images, X-ray-CT, and MRI, are static morphological images. These are useful for diagnosis of morphological disorders such as fractures, but cannot be used for functional diagnosis. Therefore, while the electrocardiograph is used for diagnosis of heart disease, the magnetic field measured using the magnetocardiograph is a vector having magnitude and direction. By obtaining the source from the magnetic field distribution around the heart, in other words, “Solving the inverse problem”, it is possible that this may one day be used to estimate the transmission route of the activity current. And, by comparing it to the electrocardiogram, it is also possible this may be used in the future to obtain useful information from the magnetic field waveform leading to diagnosis of diseases.
    In particular, it is expected to one day be used to help in the diagnosis of ischemic heart disease. Ischemic heart disease is a disease in which there is a temporary deficiency of blood flowing to the cardiac muscles, and if it becomes serious, it could lead to angina pectoris or myocardial infarction. Early discovery is difficult using an electrocardiogram, but detection may be possible in the future by temporal mapping of the magnetic field distribution using a magnetocardiograph.

    And, for newborns with congenital heart disease, discovery of the disease during the fetal stage can smooth early actions in emergency situations and the treatment process after birth.

    A fetus in a uterus is covered with a material called vernix. Vernix has high electrical insulation and shuts off almost all the current from the heart. Therefore, taking an electrocardiogram of a fetus is quite difficult and there was no way other than using an ultrasonograph (echo), which can only show shapes. On the other hand, the lines of magnetic force can pass through without being affected by vernix, which enables magnetocardiograms. Also, the magnetic field intensity weakens rapidly in inverse proportion to the square of the distance from the source, and hence it is possible that one day magnetocardiographic technology may be developed to measure the cardiac magnetic fields of the fetus only without being affected by the cardiac magnetic fields of the mother.

    Figure 8 Magnetocardiogram measurement of a fetus with a magnetocardiograph using a MR magnetic sensor (image)

    Figure 8 Potential future use of MR sensors to measure a fetus with a magnetocardiograph (image)

    Further, since this technology is expected to be capable of measuring weak magnetic fields easily and non-invasively, it may also have future applications the fields of wearable health care devices and sports science.

    Summary

    SQUID flux meters have been used measurements of biomagnetic fields, but the system itself is expensive and bulky and has basic flaws such as high running cost including the cost of periodically supplied liquid helium for cooling. As a result, it is expected that clinicians would be interested in a lower-cost and easy-to-use substitute SQUID flux meters.
    To meet such a need, TDK is developing biomagnetic sensors using compact and highly sensitive MR magnetic sensors using advanced thin-film technology and spintronics technology cultivated through the manufacture of HDD heads. Their magnetic resolution is designed to be on the order of a few tens of pT (10-11T), which is about 1000 times that of the existing MR magnetic sensors, and approaching the domain of the SQUID flux meter. Through collaborative research with the graduate school of the Tokyo Medical and Dental University, TDK has developed a prototype biomagnetic measurement system using a multi-channel MR magnetic sensor array. In 2016, we are the first organization in the world to successfully carry out proof-of-concept measurement of the cardiacmagnetic fields at room temperature, and visualization (imaging) of the cardiac magnetic field distribution.
    In 2019 and 2024, we are also the first organization in the world to successfully perform the real-time measurement of the cardiac magnetic field distribution and realize magneto-cardiometry under regular conditions (outside a magnetically shielded room), respectively.

    TDK is also working on the development of a biomagnetic field measurement system with a resolution of a few pT. By coming closer to the domain which could only be measured using a SQUID flux meter up to now, it is expected to be useful in the diagnosis of atrial diseases such as atrial fibrillation.
    Furthermore, the resolution of a few pT is at a level that is expected to have future potential uses in measuring of brain magnetic fields which are weaker than heart magnetic fields. As for biomagnetic fields, more research is being conducted on magnetoencephalograms than on magnetocardiograms. Compared to a potentiometric electroencephalograph, a magnetoencephalograph is expected to be less affected by a skull and is able to obtain sharper information. However, it is expected that a resolution of 0.5 pT or less will be required for identifying the abnormal part that generates brain wave patterns unique to patients with epilepsy, for finding causes of the serious disease ALS (Amyotrophic lateral sclerosis), and for clarifying alpha waves emitted from brains in meditation. Although this is an extremely difficult field of MR magnetic sensors, TDK will work to contribute to advanced research in biomagnetic fields by utilizing the characteristics and advantages of MR magnetic sensors.

    MR magnetic sensors from TDK have the potential to be widely used in various applications other than biomagnetic field measurement. Since they are designed to carry out measurement non-invasively and at room temperature, they can potentially be used in the field of non-destructive testing, such as magnetic particle testing (MT), to examine minute flaws that cannot be discovered by visual inspection.
    They also achieve the compactness which is characteristic of MR elements, and can also be considered for use in applications such as internal body examination devices, and artificial organs.
    Please watch out for future biomagnetic measurement systems which will be designed to carry out measurement of extremely highly sensitive biomagnetic fields easily and at low cost, and magnetic sensor technology from TDK using advanced spintronics technology.

    TDK has been working on development of MR magnetic sensors and a variety of other applications of magnetic sensor technology. These sensors are intended to be components in future-developed finished medical devices. The TDK MR sensors are not themselves finished medical devices.
    If you have any projects where the TDK MR sensor components presented in this article can be used, please feel free to get in touch with us. TDK is also planning to hold demonstrations where you can observe and also personally experience the working of a prototype biomagnetic measurement system which uses MR magnetic sensor components.

    Copyright(c) 1996-2017 TDK Corporation. All rights reserved.
    TDK logo is a trademark or registered trademark of TDK Corporation.