As seen in the strategies such as "Industry 4.0" from Germany and "Society 5.0" from Japan, the world is proactively moving forward to create new manufacturing approaches, new services, and new values using the technologies including IoT, M2M, AI, and VR. An ultra-smart society in which everything is connected via the Internet or sensor technologies is waiting for you in the near future.
TDK develops not only material technology as its core technology, but also thin-film process technology, wafer processing technology, and multilayer technology for manufacturing HDD heads, DVDs, BDs, and so on. Making full use of these technologies, TDK has developed various components for optical communication and delivered millions of optical components and devices for construction of Fiber to the Home (FTTH).
Furthermore, with the advantage of having both electronics and optics technologies, TDK has been working on miniaturization and modularization of key devices used for branch sections of optical communication networks. This article introduces the latest achievement of TDK through such efforts; the "LN thin-film" that opens up new application possibilities of LN (LiNbO3: Lithium Niobate) materials.
Technical Background
Overview of optical communication/optical transmission systems
A new evolutionary stage has begun for optical communication networks to process explosively increasing traffic resulting from the spread of the Internet and associated high speed transmission of large capacity content. In data centers, reduction of enormous electrical power consumed by communication equipment and air conditioning is problematic for the future growth of the cloud computing, Internet of Things (IoT), and machine-to-machine (M2M). Optical transmission systems featuring low power dissipation and high-speed large capacity transmission are being introduced to overcome these problems.
Clearly, the performance of next generation optical communication/optical transmission devices will depend on various optical transmission equipment and the performance and quality of the optical components within such devices. As networks and systems expand, the scale of optical transmission devices will grow larger, and the number of installations will increase in parallel. Therefore, the importance of saving space and power through miniature and high-density packaging will grow more and more. At the same time, optical components are evolving into modularized and/or arrayed ones, and further into optical integrated circuit instead of merely miniaturizing conventional discrete optical components.
The configuration of a typical optical communication network is shown in Fig. 1. The backbone network is comprised of a core network that connects towns and cities, as well as an urban area sized metropolitan network. The subscriber accesses networks such as FTTH (Fiber to the Home) branch from the metropolitan network.
In an optical communication system, various advanced technologies such as digital coherence, DWDM (Dense Wavelength Division Multiplexing), and ROADM (Reconfigurable Optical Add-Drop Multiplexer) have been introduced to realize power-savings and to improve the economics of high-speed and large-capacity transmission networks.
DWDM : Dense Wavelength Division Multiplexing ROADM : Reconfigurable Optical Add-Drop Multiplexer
Fig. 1 Configuration of Optical Communication Network
Key technologies that contributed to development of optical communication systems
Long distance communications using optical fibers has been feasible since the 1970s when low-loss optical fiber was invented following semiconductor lasers and photo-diodes; these three fundamental technologies enabled optical communications. The first generation of practical optical communication systems were developed in the 1980s, and the second generation appeared in the decades of the 1990s and 2000s. The third generation is now under way.
Key technologies resulted in advances of the optical communication system are as follows:
- PLC (Planar Lightwave Circuit)
A PLC is a device in which an integrated optical waveguide is fabricated onto a flat substrate using photolithographic processes similar to methods established by the LSI industry. The optical waveguides have similar transmission characteristics as optical fibers. Transmission in an optical fiber is based upon differences in the refractive index. In the1980s, the fundamental technologies were researched, and by the 1990s practical PLC devices such as an AWG (Arrayed Waveguide Grating) were developed.
- Optical Amplifier / EDFA (Erbium-doped Fiber Amplifier)
Though transmission losses in optical fibers are very low, since they cannot be avoided, relays need to be installed in long-distance transmissions. An optical amplifier is a device for boosting optical signal levels without the need to perform optical to electrical conversions. The optical amplifier uses a special optical fiber containing the element of erbium (Er), is referred to as an EDFA (Erbium-doped fiber amplifier). The EDFA is critical to realize long distance transmission such as the transoceanic optical cables.
- WDM (Wavelength Division Multiplexing) Technology
WDM is a technology that combines signals of multiple wavelengths onto a single optical fiber for long distance transmission. DWDM (Dense WDM: Dense Wavelength Division Multiplexing) technology further improves upon WDM technology by allowing an extremely large numbers of wavelength (and therefore an extremely large amount of data) to be transmitted by a single optical fiber.
- AWG (Arrayed Waveguide Grating)
A signal multiplexed by WDM/DWDM technology has to be separated (branched) into individual channels having the original plurality of wavelengths at the receiving side of an optical terminal. The AWG is an optical device that plays a role as an optical multiplexer/demultiplexer. The AWG was developed on PLC technology platform in 1990s.
- ROADM (Reconfigurable Optical Add-Drop Multiplexer)
A ROADM is a device that instantly and flexibly creates optical paths for optical signals of certain wavelength in an optical fiber communication network by software. With ROADM, flexible and efficient network operation that enables high-speed transmission of large-capacity data is feasible by controlling the drop, add, and through conditions of optical paths remotely to form virtual detours and new networks.
- OXC (Optical Cross Connect)
OXC is a network connection technology evolved from ROADM. By employing large-scale optical switches, OXC devices used for branch or other sections in mesh core networks can cross-connect large-capacity signals without converting them.
- Digital Coherent Optical Transmission technology
Digital Coherent Optical Transmission is a technology which allows highly reliable long-distance transmission of extremely large data capacity within a single optical fiber. It is achieved by introducing advanced digital signal processing (DSP) technology into the optical communication scheme. It is one of the key technologies for realizing near-future optical communication networks.
- WSS (Wavelength Selective Switch)
A WSS is an optical device that switches and sorts a wavelength multiplexed optical signals. It allows network operators to direct discrete wavelengths to specific output ports on the order of milliseconds. Key components of the WSS are optical multiplexer/demultiplexer, an MEMS mirror, input/output fibers, etc. It is an advanced technology commonly used for sophisticated ROADM systems.
Through various technical innovations, FTTH has also become widely deployed since initial deployments began shortly after the Year 2000. In parallel, an optical communication network has evolved that serves as the infrastructure that supports the ICT society. Fig. 2 shows the transition of optical communication technology correlated the expansion of transmission capacity.
Fig. 2 Progress in Optical Communication Technology and Transition of Transmission Capacity
Various Optical Components and Devices Supporting Optical Communication/Optical Transmission Systems
As the optical communication network expands beyond the core and metropolitan networks and the optical transmission systems in data centers evolve with the growth of the cloud computing, the performance, quality, and reliability of optical components and devices used for interconnection, branching, and amplification have become extremely important. Such interconnection, branching, and amplification components and devices have become as critical to network operation as the fundamental elements (namely the semiconductor laser, the photo diode, and the optical fiber) are.
The primary optical components and devices that support the optical communication/optical transmission system are as follows:
Table 1: Primary optical components and optical passive components used for optical communication system
Optical connector |
When connecting optical fibers to each other, minute core sections through which the light passes are butted together. An optical connector is an optical component mounted onto the end of an optical fiber to facilitate the alignment and connection between fibers. |
Optical splitter |
An optical splitter is an optical component for branching a single optical fiber into multiple optical fibers. In FTTH, 1x32 splitter, 1x8 splitter, and 1x4 splitter are commonly used. |
Optical isolator |
When light is reflected on the interface of the connected sections of an optical communication system, back reflected light may occur resulting in false operation and line noise. An optical isolator allows only one-way passage of light to prevent back reflections. |
Optical switch |
An optical switch is component for switching the path of an optical signal. Switching may be realized mechanically, by electro-optical effect, or thermo-optic effect. |
Optical Multiplexer / Demultiplexer |
An optical multiplexer / demultiplexer combines optical signals of multiple wavelengths into a single optical fiber and demultiplexes (separates) the transmitted optical signal to single wavelengths onto individual fibers. The optical multiplexer / demultiplexer is a critical component in optical WDM (wavelength multiplexed)/DWDM (high density WDM) systems. |
Optical integrated circuit |
An optical integrated circuit is a device into which multiple components such as semiconductor lasers and optical switches are integrated on a substrate. LSI manufacturing technologies such as CVD and photolithography are utilized to fabricate such devices. |
Optical fiber array |
An optical fiber array is a device for precisely arranging multiple optical fibers and connecting them to the optical waveguides of an optical splitter and so on. To minimize transmission loss, extremely advanced high-precision processing technology and assembly technology are required. |
Optical modulator |
An optical modulator is a device that converts an electric signal to an optical signal. Some optical modulators make use of an electro-optic effect of EO polymers or ferroelectric materials such as LN (Lithium Niobate). |
Tap-PD module |
Tap-PD module is an optical power monitor that measures the intensity of the optical signals using photo detectors (PD), after tapping some input signals transmitted via optical fibers. There is a growing need for arrayed miniature Tap-PD modules. |
TDK's Advantage in Optical Component and Device Technologies
Several millions of optical components are delivered for construction of FTTH networks
TSince the beginning of 1990s, TDK has developed and commercialized various optical components, including optical isolators.
The optical isolator uses a phenomenon called Faraday rotation to cancel the influence of reflected light (return light) to make only forward directed optical signal pass through the device. Along with the optical splitter, the optical isolator has been designed into many optical communication systems including FTTH networks.
Various technologies which differ from those of electronic component manufacturing are necessary for the commercialization of optical components and devices. TDK can advantageously draw upon a comprehensive set of core technologies accumulated over many years including know-how in the following disciplines:
materials technology,process technology,evaluation and simulation technology、device and module technologyandproduction engineering .
TDK technologies supporting optical communication/optical transmission technology are collectively introduced as follows;
- A unique, comprehensive set of technical capabilities based on the accumulated core technologies
HDD heads are manufactured by forming nanometer order head elements on a wafer making use of highly advanced thin-film processing technology. The next generation of HDDs will utilize a laser mounted thermal assist magnetic head.
» » Related Information: Five core technologies of TDK
Fig. 3 Structure of TMR Element of HDD Head and Principle of Thermal Assist Magnetic Recording
- Production engineering that optimizes QCD (Quality, Cost, and Delivery) in the most effective way
In an optical communication/transmission system, the number of relays and branch sections increases as a network and/or system expands. Therefore, the quality and performance of the optical components and devices used within the system have an ever-increasing effect on the performance of the entire network. TDK's production engineering optimizes QCD (Quality, Cost, and Delivery) though manufacturing experience of electronic components and devices such as HDD heads and multilayer ceramic chip capacitors and provides the high standard of quality and reliability required for the manufacture of optical components and devices. This includes the optical fiber arrays produced by TDK.
- In-house manufacturing of production and inspection apparatuses
TDK has not only developed a unique manufacturing method of electronic components and devices including capacitors and inductors, but also manufactured many manufacturing equipment in-house for commercialization. In the development of various optical components and devices, many manufacturing and inspection equipment are manufactured in-house.
Next Generation Optical Components/Optical Modules That TDK Strives For
With the prevalence of the Internet and smartphones and the evolution of IoT and M2M, communication traffic has explosively increased over the past several years and will continue to grow into the future. In order to manage such explosive growth, the optical communication system is migrating into the era of terabit (Tbps) transmission and petabit (Pbps) transmission. In data centers and high performance computing (HPC), interconnections for transmitting electrical signals remain the bottleneck. The developments of solutions that connect devices and circuits by optical transmission system are progressing and further advancement of advanced technologies such as silicon photonics (Si photonics) technology is expected.
In preparation for a next generation optical communication/optical transmission system, not only miniaturization, high integration, and energy saving but also excellent quality, performance, and reliability are required for optical components and devices.
Based on the thin-film processing technology, wafer processing technology, multilayer technology, nanometer order ultra-precision processing technology, and ultra-precision packaging of micro optics components cultivated by manufacturing HDD heads, DVDs, and BDs, TDK has successfully developed "LN crystalline thin-film." The product is expected to make a significant contribution to miniaturization, space saving, and cost reduction of optical communication/transmission devices.
A "LN crystalline thin-film" is an application of LN (LiNbO3: Lithium Niobate), an optical material commonly used for devices such as optical modulators and optical switches, which is realized based on the thin-film processing technology instead of single crystal pull-up method. Since LN thin-films have advantages compared to the crystal pull-up method in terms of mass productivity and cost and are highly compatible with semiconductor or other thin-film electronic components, they can be used for various applications in addition to optical components and devices.
Request for Information, Delivery of Samples
We accommodate the various needs of our customers
Please feel free to contact us through the inquiry link below for information concerning "LN thin-film", characteristics, specifications, or customization of shapes.