TDK Product Information NEWS Vol.061 December 2021
Topics
・Two contents for myTDK Members-only have been released
・Application Note "Ag-Stacked Transparent Conductive Film" has been released
・Featured Stories "Stop Looking: The Power of Indoor Positioning Based on Geomagnetism" has been released
Two contents for myTDK Members-only have been released
❙ PTM (Product Training Module) Chip Beads
Introducing the features and functions of TDK chip beads and the points of selection.
》 "PTM (Product Training Module) Chip Beads" (myTDK Members-only)
❙ Examples of Countermeasures Using a Power Supply Line Common-Mode Filter
As the safety and convenience of automobiles increases, more electronic devices are being used in vehicles. Electronic circuits have signal lines and power supply lines, and both require noise countermeasures. Here, we present examples of countermeasures based on data measured using a TDK power supply line common-mode filter.
》 "Examples of Countermeasures Using a Power Supply Line Common-Mode Filter" (myTDK Members-only)
Application Note "Ag-Stacked Transparent Conductive Film" has been released
TDK's transparent conductive silver [Ag] alloy film (FleClear®) is a versatile material that has numerous use cases. Many of these uses require making direct electrical contact to the film's low resistance conductive surface in order to adequately perform the targeted applications. The following Application Note provides an overview of FleClear®, a step-by-step procedure of attaching an metal electrode, a list of needed equipment, along with the recommended materials to attach copper bus bars to the conductive surface. Additionally, where important, the suppliers and the respective numbers, are also listed..
》 Ag-Stacked Transparent Conductive Film
Featured Stories "Stop Looking: The Power of Indoor Positioning Based on Geomagnetism" has been released
Droves of people come and go at hospitals and offices. Mountains of packages and materials are stored at warehouses and factories. At many facilities, efforts are being made to streamline tasks and ensure personnel safety by tracking and managing the locations of people and objects. TDK offers a groundbreaking solution that leverages geomagnetism—which exists everywhere—to enable highly precise, indoor positioning of people, objects and powered vehicles in real time over broad areas, helping to improve business operations.
》 Stop Looking: The Power of Indoor Positioning Based on Geomagnetism