Q.
What are the effects of use with the input/output side changed?
- EMV-Bauelemente >
- EMV-Netzfilter
A. If the circuit is the input/output symmetric type, there is no difference in performance characteristics. However, for the asymmetric type, there can be some difference in attenuation characteristics on the actual device.