FAQ
Q.
Can mounting chip beads for the low-frequency band in series with the chip beads for the GHz band allow the obtaining of both characteristics? Also, should there be any problems if multiple chip beads are mounted in series?
  • EMV-Bauelemente
  • >
  • Chip Beads


A. Both characteristics can be obtained by connecting them in series. (It will be as if two electrical characteristics are overlayed.) A disadvantage is that the series resistance value rises and the voltage drop occurs.