FAQ
Q.
Is it possible to operate with a substrate which is different from the one shown in the data sheet?
  • HF-Komponenten
  • >
  • Chip-Antennen


A. There is no adverse effect on chip antenna action even in the case of differing conditions such as the material or thickness of the board being used.