News

TDK Product Information NEWS Vol.024 July 2018
 
TDK Corporation delivers monthly product information to you.
 

 
Topics
 
  • Three new InvenSense products have been released
  • Capacitors Selection Guide has been released
  • Product Overview for Automotive Series has been released
 
Three new InvenSense products have been released
 

TDK has added three InvenSense products, which include motion sensors, capacitive pressure sensors, and MEMS microphones, to our Product Center. Our technical support tools also include various tools related to InvenSense, which can provide valuable assistance with product development.

 
 
Motion Sensors

TDK delivers Motion Interface solutions with fully integrated sensors and robust firmware algorithms. Our devices enable our customers to integrate Motion Interface capability directly into devices with minimal development cost and effort.

Motion-based devices from TDK are rapidly becoming a key function in many consumer electronic devices including mobile, wearable, Smart Home, and automotive and industrial devices.

Our motion solutions, including gyroscopes, accelerometers, compasses and pressure sensors, detect and track an object's motion in three-dimensional space, allowing consumers to interact with their electronic devices in free space.

》Product Portal

 
 
Capacitive Pressure Sensors

TDK delivers Motion Interface solutions with fully integrated sensors and robust firmware algorithms. Our devices enable our customers to integrate Motion Interface capability directly into devices with minimal development cost and effort.
Motion-based devices from TDK are rapidly becoming a key function in many consumer electronic devices including mobile, wearable, Smart Home, and automotive and industrial devices.

Our motion solutions, including gyroscopes, accelerometers, compasses and pressure sensors, detect and track an object's motion in three-dimensional space, allowing consumers to interact with their electronic devices in free space.

》Product Portal

 
 
MEMS Microphones

TDK's MEMS microphones have achieved compact, low-profile, and high in performance due to the CSMP (chip size MEMS package) technology that has been cultivated through the development of products such as SAW devices.

TDK and InvenSense's analog and digital microphone portfolios build on a strong heritage of industry firsts, including continuous improvement of MEMS microphone SNR, ever-higher integration levels, and even lower power consumption. Technological advances like these have enabled machine speech recognition & adaptive noise suppression to become commonplace in consumer devices and other applications.

Humans intuitively understand audio capture to be a critical factor in awareness of their surroundings. Voice capture is quickly becoming the leading interface between man and machine. InvenSense is microphones are first in line to enable smart devices with accurate voice collection. InvenSense combines the capability to sense audio along with a wide sensor portfolio, capturing motion, pressure, air quality and ultrasonic information.

》Product Portal

 
Capacitors Selection Guide has been released
 

It includes a product map organized by capacitance and rated voltage, and information such as the features of each capacitor type.

》Capacitors Selection Guide

 
Product Overview for Automotive Series has been released
 

We have prepared narrated a presentation about TDK's automotive series MLCC for busy engineers to understand product features and quality in short time.

》List of Product Overviews for Automotive Series

Automotive Grade / CGA Series General (Up to 50V)
ADAS ECU Power Supply Circuit Applications Vol.1

Here, we will use the example of ADAS (Advanced Driver Assistance Systems) to describe the excellent characteristics and high reliability of the CGA series of capacitors with a rated voltage of 50V or less.
In volume 1, we will describe high capacitance capacitors used for decoupling.
Automotive Grade / CGA Series General (Up to 50V)
ADAS ECU Power Supply Circuit Applications Vol.2

In volume 2, we will describe high capacitance capacitors used for smoothing.
Automotive Grade / CGA Series Mid Voltage (100 to 630V)
xEV Higher Withstand Voltage Applications

Here, we will describe the excellent characteristics and wide product range of our automotive grade / CGA series capacitors with mid-level rated voltages (rated voltages from DC 100V to 630V), and applications for which they can be used.
Automotive Grade / CGA Series High Voltage (1,000V and over)
xEV Wireless Charger Resonant Circuit Applications

Here, we use the example of wireless charging for electric vehicles to describe the excellent characteristics and wide product range of the automotive grade CGA series of high voltage capacitors with a rated voltage of 1,000V or more.
Automotive Grade / CGA Series Soft Termination
Same Footprint with Crack Countermeasures

Here, we will describe the terminal electrode structure of automotive grade soft termination products and their excellent characteristics, and present applications where they can be used.
Serial Design / CEU Series
Special Short Preventing Structure in case of Cracking

Here, we will describe the internal structure and excellent characteristics of the serial design CEU series and present applications where they can be used.