Q.
What is the difference between S-parameters and Netlists?
- Kondensatoren /
- Induktivitäten (Spulen) /
- EMV-Bauelemente /
- HF-Komponenten /
- Schutzbauelemente /
- Übertrager >
- Keramik-Vielschichtkondensatoren (MLCC) /
- 3-Leiter-Durchführungskondensatoren /
- Chip Beads /
- 3-Leiter-Durchführungsfilter /
- Entstörfilter /
- Balun /
- Leistungsteiler / Splitter /
- Chip Varistors / Ceramic Transient Voltage Suppressors /
- Impuls-Übertrager und LAN Module
A.
S-parameters can be used to explain the amount reflection and transmission when a signal is given to a component that is used as a black box.
A Netlist contains equivalent circuit information that can be read using a simulator after a component is made as an equivalent circuit.
Usually, Netlists are used for analyzing time domains such as transient analysis. S-parameters are used for analyzing frequencies.
S-parameters use actually measured values, while Netlists themselves are equivalent circuit models and actually measured values are often different from the Netlist, especially in the high-frequency range.