Q.
Do the products meet the EN/IEC61000-4-5 lightning surge test?
- EMV-Bauelemente >
- EMV-Netzfilter
A. It depends on the required level. However, the lightning surge test is basically not considered in the design of the products. Use the products within the rating. If there is a possibility that voltage beyond the rating may be applied, use of surge absorbers such as varistors and arresters should be considered.