FAQ
Q.
The data sheet has specifications on “rated currents” but not on “rated voltages”. Should there be no problems during use as long as the current values are conformed to?
  • EMV-Bauelemente
  • >
  • Chip Beads


A. There is no problem with chip beads when used within the scope of rated current. Therefore, there are no tolerance specifications for insulation breakdown.