FAQ
Q.
Would it be a problem to use inductors in parallel?
  • Induktivitäten (Spulen)


A. It is possible to use inductors in parallel.
When inductors are used in parallel, a greater amount of current can flow.
However, there is the disadvantage that inductance will decrease, as it is a synthetic inductance.
The synthetic inductance Lt can be obtained using the following formula: