Application Note

Noise Suppression Sheet IFL Series "Flexield"

Use Case in Compact Electronic Devices
such as Smartphones

Use Case in Compact Electronic Devices such as Smartphones

Flexield is a simple and effective solution for the problem of "self-poisoning" which is an EMC problem in electronic devices.

With increasing density of the printed circuit board, the noise environment has also deteriorated in compact electronic devices

Use case of the noise suppression sheet "Flexield" from TDK (Abbreviated simply to "Flexield" below), and its effectiveness in compact electronic devices are presented below.
Merely meeting various EMC specifications is not enough to suppress noise in electronic devices. Especially in multi-functional compact electronic devices with communication functions such as smartphones, with increasing density of the printed circuit board, the noise emission produced internally interferes with the antenna and causes a drop in reception sensitivity as well as a degradation in image and voice quality. A solution needs to be found for this problem of "self-poisoning" which is an EMC problem inside the device.
Figure 1 shows the block diagram and basic internal structure of a smartphone. It consists of the main circuit board on which IC circuits such as the application processor and power management IC are mounted, a sub-circuit board which is connected to the display, and the camera module, and they are connected using flexible cables (FPC/FFC).

Figure 1  Block diagram and internal structure of a smartphone
Figure 1 Block diagram and internal structure of a smartphone

Major causes of noise emission inside smartphones

The application processor which is central to the smartphone, and which is becoming increasingly multi-functional, is an SoC (System-on-a-chip) into which multiple ICs have been integrated. The flexible cables and connectors which connect the SoC and the peripheral circuits (power inductors, etc.), as well as the main circuit board and sub-circuit board, are the main sources of noise emission which is the cause of "self-poisoning" in smartphones.
Flexield from TDK is a thin and flexible noise suppression sheet, and by cutting it to the desired shape and pasting it, it functions as a simple and effective noise suppression mechanism (Figure 2).

Figure 2  Major places where Flexield is used in a smartphone
Figure 2 Major places where Flexield is used in a smartphone

It offers a state-of-the-art EMC solution using simulation technology.

Representation of the distribution of noise emission intensity by the near electromagnetic field measurement

Noise emission consists of electromagnetic waves which are conducted across space through the interaction between the electrical field and magnetic field. However, near the source of noise emission, the electrical field and magnetic field exist independently with either being dominant. This area is known as the near field. In specific terms, the area which is at a distance of less than λ/2π (λ: wavelength) from the emission source is the near field, and the area which is a distance of more than λ/2π is the far field. Since the value of λ/2π is approximately 5cm at 1GHz, in compact electronic devices such as smartphones, it is necessary to understand the distribution of the electrical field and magnetic field in the near field. The near field measurement system is used for this purpose. In this system, an electromagnetic field probe is brought close to the DUT (device under test) such as the printed circuit board, and it scans the device while maintaining a fixed gap, and the data obtained is used to represent the distribution of noise intensity (Figure 3). Simulation technology, which is one of the core technologies of TDK, is used as a solution for various noise problems such as the "self-poisoning" problem.

Figure 3  Configuration of a near electromagnetic field measurement system
Figure 3 Configuration of a near electromagnetic field measurement system

It suppresses noise emission not just in the ICs, but over a wide area which includes peripheral circuits.

Power inductors are also a cause of noise emission

Figure 4 shows an example of the distribution of the magnetic field intensity of the IC peripheral circuits of the main circuit board in a smartphone, measured using the near electromagnetic field measurement system. The area with high noise level is shown in red, while the area with low noise level is shown in blue. In the absence of any measures, the red area is widely distributed around the application processor and power management IC, but when Flexield is installed, the noise level is considerably reduced. Since the noise is emitted not only from the ICs, but also from the power inductors, installation of Flexield in the IC peripheral circuit is an extremely effective noise suppression measure.

Figure 4  Example of the effectiveness of noise suppression in the IC peripheral circuit of the main circuit board
Figure 4 Example of the effectiveness of noise suppression in the IC peripheral circuit of the main circuit board

Flexield is extremely effective in suppressing noise even in flexible cables.

The cabling and wiring pattern functions as an antenna which emits noise

The wiring patterns of the cable or of the printed circuit which transmit high frequency current function as an antenna which emits noise. Figure 5 is an example of the effectiveness of noise suppression when a flexible cable is used to connect the main circuit board and sub-circuit board. It is clear from the near magnetic field measurement that in the absence of any measures, an extremely high level of noise is emitted.
Since Flexield is thin and flexible, it has the advantage of being able to be easily attached even to flexible cables. By installing Flexield, there has been considerable suppression of intense noise.

Figure 5  Example of effectiveness of noise suppression in flexible cables
Figure 5 Example of effectiveness of noise suppression in flexible cables