Tech Library Products & Technologies Applications & Cases (-) Solution Guides Facet Tech Note List Article Category » Taxonomy term » Name Drahtlose Energieübertragung EMV-Bauelemente HF-Komponenten Induktivitäten (Spulen) Kondensatoren Schirmungsfolien / Magnetfolien Schutzbauelemente Sensoren und Sensorsysteme Facet Tech Note List Product Categories L1 Automobilindustrie ICT Industrie & Energie Medizin & Gesundheitswesen Unterhaltungselektronik Wearables Facet Tech Note List Application Category 2023 2022 2021 2020 2019 2018 2017 2016 2015 Facet Tech Note List Published on Date Solution Guides März. 2023 [Solution Guide] Noise Countermeasures for DC-DC Converter Input Lines using 3-terminal Filters (Feed-through Filters for Power Lines) New In recent years, switching speed of DC-DC converters has increased as the switching frequency has become higher. As a result, high-frequency noise is generated when inductance and stray capacitance of the wiring of board or inside IC resonate due to a sudden change in input current. The high-frequency noise can conduct to external circuits and cause abnormal operation of the set. This Solution Guide introduces examples of noise countermeasures using a three-terminal filter (feed-through filter for power lines) with low ESL, which is effective for noise countermeasures against noise generated on the input side of DC-DC converters. In recent years, switching speed of DC-DC converters has increased as the switching frequency has become higher. As a result, high-frequency noise is generated when inductance and stray capacitance of the wiring of board or inside IC resonate due to a sudden change in input current. The high-frequency noise can conduct to external circuits and cause abnormal operation of the set. This Solution Guide introduces examples of noise countermeasures using a three-terminal filter (feed-through filter for power lines) with low ESL, which is effective for noise countermeasures against noise generated on the input side of DC-DC converters. EMV-Bauelemente EMV-Bauelemente 3-Leiter-Durchführungsfilter Solution Guides März. 2023 [Solution Guide] Solution Guide: Replacing Electrolytic Capacitor with MLCC, Revised Guide Update Traditionally, aluminum electrolytic capacitors and tantalum electrolytic capacitors have been widely used for smoothing and decoupling applications that require large capacitance. With increasing capacitance values, MLCCs are replacing various electrolytic capacitors in power circuits and other applications. Replacing electrolytic capacitors with MLCCs offers various benefits such as space reduction due to smaller size and lower profile, reduced ripple voltage due to low ESR, and improved reliability due to reduced self-heating. On the other hand, low ESR, which is an advantage of MLCCs, can sometimes lead to abnormal oscillation or anti-resonance. Additionally, high dielectric constant MLCCs (Class 2) exhibit a characteristic capacitance change when DC voltage is applied, so caution is necessary. This guide explains the advantages and precautions to be taken when replacing electrolytic capacitors with MLCCs. Traditionally, aluminum electrolytic capacitors and tantalum electrolytic capacitors have been widely used for smoothing and decoupling applications that require large capacitance. With increasing capacitance values, MLCCs are replacing various electrolytic capacitors in power circuits and other applications. Replacing electrolytic capacitors with MLCCs offers various benefits such as space reduction due to smaller size and lower profile, reduced ripple voltage due to low ESR, and improved reliability due to reduced self-heating. On the other hand, low ESR, which is an advantage of MLCCs, can sometimes lead to abnormal oscillation or anti-resonance. Additionally, high dielectric constant MLCCs (Class 2) exhibit a characteristic capacitance change when DC voltage is applied, so caution is necessary. This guide explains the advantages and precautions to be taken when replacing electrolytic capacitors with MLCCs. Kondensatoren Keramik-Vielschichtkondensatoren (MLCC) Solution Guides Nov. 2022 [Solution Guide] Flying Capacitors in PV Booster stages One of the well-established key requirements in solar inverters is their high efficiency. But also, their costs, size and weight are subject to continuous improvements. One approach to better fulfil all these demanding requirements simultaneously is the use of multilevel topologies. The main advantages of switching between multiple voltage levels are lower voltage stress for the semiconductors and lower ripple stress for the power chokes. This means that lower-voltage semiconductors can be used, which are typically cheaper. Lower ripple stress for the chokes makes smaller and thereby lighter and cheaper choke designs possible. The flying capacitor topology is a multilevel topology, that is an interesting choice especially for (but not limited to) the booster stage of a solar inverter. As its name implies, it needs a capacitor as a key element. This article describes and compares possible TDK solutions therefor. One of the well-established key requirements in solar inverters is their high efficiency. But also, their costs, size and weight are subject to continuous improvements. One approach to better fulfil all these demanding requirements simultaneously is the use of multilevel topologies. The main advantages of switching between multiple voltage levels are lower voltage stress for the semiconductors and lower ripple stress for the power chokes. This means that lower-voltage semiconductors can be used, which are typically cheaper. Lower ripple stress for the chokes makes smaller and thereby lighter and cheaper choke designs possible. The flying capacitor topology is a multilevel topology, that is an interesting choice especially for (but not limited to) the booster stage of a solar inverter. As its name implies, it needs a capacitor as a key element. This article describes and compares possible TDK solutions therefor. Kondensatoren Folien-Kondensatoren CeraLink®-Kondensatoren Metallisierte Polypropylene-Kondensatoren (MKP/MFP) Solution Guides Dez. 2021 [Solution Guide] MLCC Solutions for Power Supply Circuits (Verification of Optimal Structures for Output Capacitors) In the automotive field, CPUs and FPGAs for systems that require advanced image processing, such as onboard ADAS ECUs and autonomous ECUs, need to operate at high speed and require high drive current in conjunction with the increasing performance and functionality of systems. Also, in the ICT field, power supply configurations that support higher current required for devices that need huge amounts of power such as servers. There is a trend towards higher operating speeds and higher currents in the power supply lines of systems with increased performance and functions as described above. At the same time, power supply structures that maintain the nominal voltage within narrow tolerance ranges, which have decreased in conjunction with processor miniaturization, are also required. In the automotive field, CPUs and FPGAs for systems that require advanced image processing, such as onboard ADAS ECUs and autonomous ECUs, need to operate at high speed and require high drive current in conjunction with the increasing performance and functionality of systems. Also, in the ICT field, power supply configurations that support higher current required for devices that need huge amounts of power such as servers. There is a trend towards higher operating speeds and higher currents in the power supply lines of systems with increased performance and functions as described above. At the same time, power supply structures that maintain the nominal voltage within narrow tolerance ranges, which have decreased in conjunction with processor miniaturization, are also required. Kondensatoren Keramik-Vielschichtkondensatoren (MLCC) Solution Guides Sep. 2021 [Solution Guide] Sensors solutions that enable advanced control of service robots Service robots are widely used in various situations such as logistics / transport, security, cleaning, housework, hobbies / entertainment and care / assistance. Since service robots are used in a wide variety of situations, it is necessary to fulfil many requirements such as smooth communication with humans (HMI), ensuring safety and responding to changes in the real time. In service robots, the role of a sensor is very important. In this article, we will take a vacuum cleaner robots as an example. Service robots are widely used in various situations such as logistics / transport, security, cleaning, housework, hobbies / entertainment and care / assistance. Since service robots are used in a wide variety of situations, it is necessary to fulfil many requirements such as smooth communication with humans (HMI), ensuring safety and responding to changes in the real time. In service robots, the role of a sensor is very important. In this article, we will take a vacuum cleaner robots as an example. Sensoren und Sensorsysteme Bewegungssensoren / Inertialsensoren Drucksensoren Temperatursensoren (NTC) Ultraschallsensoren Embedded Motor-Controller IMU (Inertial Measurement Unit) Luftdrucksensoren MEMS-Mikrofone (Mikrofon) NTC-Elemente NTC-Sensor-Systeme SMD-NTC-Thermistoren (Sensoren) Time-of-Flight (ToF) Ultraschallsensoren Solution Guides Nov. 2020 [Solution Guide] Gesamtlösungen für NFC-Schaltungen NFC ist eine Abkürzung für Near Field Communication; es handelt sich um eine Art drahtloser Kommunikation mit kurzer Reichweite. NFC ist eine Funktion, die Datenkommunikation und Authentisierung durchführen kann, wenn zwei NFC-kompatible Geräte in die Nähe zueinander gebracht werden, und ihr Einsatz in Smartphones hat in den letzten Jahren stark zugenommen. Auch in Peripheriegeräten einschließlich tragbarer Endgeräte, wie z.B. Smart-Uhren, ist ein zunehmender Einsatz von NFC zu beobachten. NFC wird in vielen Situationen eingesetzt, u.a. beim bargeldlosen Bezahlen und bei der Authentifizierung von Verbindungen mit Peripheriegeräten, und es wird erwartet, dass es auf dem Weg zu einer berührungslosen Gesellschaft für noch vielfältigere Anwendungen eingesetzt werden wird. Dieser Artikel stellt die wichtigsten Komponenten vor, die in NFC-Schaltungen verwendet werden: NFC-Antenne, Magnetblech, LC-Filterinduktivität, Ein-End-Schaltungsbalun und elektrischer Doppelschichtkondensator (EDLC/Superkondensator). NFC ist eine Abkürzung für Near Field Communication; es handelt sich um eine Art drahtloser Kommunikation mit kurzer Reichweite. NFC ist eine Funktion, die Datenkommunikation und Authentisierung durchführen kann, wenn zwei NFC-kompatible Geräte in die Nähe zueinander gebracht werden, und ihr Einsatz in Smartphones hat in den letzten Jahren stark zugenommen. Auch in Peripheriegeräten einschließlich tragbarer Endgeräte, wie z.B. Smart-Uhren, ist ein zunehmender Einsatz von NFC zu beobachten. NFC wird in vielen Situationen eingesetzt, u.a. beim bargeldlosen Bezahlen und bei der Authentifizierung von Verbindungen mit Peripheriegeräten, und es wird erwartet, dass es auf dem Weg zu einer berührungslosen Gesellschaft für noch vielfältigere Anwendungen eingesetzt werden wird. Dieser Artikel stellt die wichtigsten Komponenten vor, die in NFC-Schaltungen verwendet werden: NFC-Antenne, Magnetblech, LC-Filterinduktivität, Ein-End-Schaltungsbalun und elektrischer Doppelschichtkondensator (EDLC/Superkondensator). Drahtlose Energieübertragung HF-Komponenten Induktivitäten (Spulen) Kondensatoren Schirmungsfolien / Magnetfolien Doppelschichtkondensatoren (EDLC / Supercapacitors) Induktivitäten (Spulen) Drahtlose Energieübertragung / NFC-Antennen (Schild) Solution Guides Okt. 2020 [Solution Guide] Burst noise countermeasures using ESD Notch Filters and Noise Suppression Filters Entstörfilter Kerbfilter mit ESD-Schutzfunktion Solution Guides Okt. 2020 [Solution Guide] Sound distortion countermeasures using ESD Notch Filters and Noise Suppression Filters EMV-Bauelemente Entstörfilter Kerbfilter mit ESD-Schutzfunktion Solution Guides Dez. 2019 [Solution Guide] Soft Termination Capacitors, Inductors, and Chip Beads for High-Reliability Products for Automotive Applications Automakers are incorporating more multifunctional capabilities into automobiles as they seek to make autonomous driving a reality. Electronic control units (ECUs) for advanced driver assistance systems are consuming more power, and the latest trend is toward ECU integration—installing an ECU close to the engine room or other working part. Automakers are incorporating more multifunctional capabilities into automobiles as they seek to make autonomous driving a reality. Electronic control units (ECUs) for advanced driver assistance systems are consuming more power, and the latest trend is toward ECU integration—installing an ECU close to the engine room or other working part. EMV-Bauelemente Induktivitäten (Spulen) Kondensatoren Induktivitäten (Spulen) SMD / SMT-Induktivitäten (Spulen) Solution Guides Juli. 2019 [Solution Guide] Ensuring communication quality and filtering suitable for PoC (Power over Coax) With the increasing speed and sophistication of interfaces in cars, the PoC (Power over Coax) approach is gaining in popularity, as it allows superimposing signals and power in one coaxial cable, for example for LVDS based automotive camera systems. A PoC filter consisting of one or more inductors and chip beads is used on the circuit side to separate the signal and the power supply current. This is important in terms of maintaining communication quality. The PoC filter therefore requires inductors that realize high impedance for AC components over a wide bandwidth range from low to high frequencies. With the increasing speed and sophistication of interfaces in cars, the PoC (Power over Coax) approach is gaining in popularity, as it allows superimposing signals and power in one coaxial cable, for example for LVDS based automotive camera systems. A PoC filter consisting of one or more inductors and chip beads is used on the circuit side to separate the signal and the power supply current. This is important in terms of maintaining communication quality. The PoC filter therefore requires inductors that realize high impedance for AC components over a wide bandwidth range from low to high frequencies. Induktivitäten (Spulen) Chip Beads SMD / SMT-Induktivitäten (Spulen) Seitennummerierung Aktuelle Seite 1 Seite 2 Seite 3 Nächste Seite Next › Letzte Seite Last »