- Kondensatoren >
- Bedrahtete Keramik-Vielschichtkondensatoren (MLCC)
A.
It means self-induced heating exceeds 20°C. Often when such use with a power circuit can be assumed in a case where such a large ripple current occurs. Normally, many components that generate more heat such as a power IC and transformer are peripherally placed. Therefore, there is the danger of the temperature of the capacitor coupled with self-heating exceeding the upper limit of the operating temperature. Continued use of an capacitor that has exceeded the upper limit of its operating temperature leads not only to lowered capacitance, but also to accelerated life deterioration, and in the worst case, short-circuit failure. Please be sure to use an capacitor within the allowable ripple current.
>>MLCC with Dipped Radial Lead
For any other product-related questions or inquiries, please contact us throughone of our sales representatives or this website.