Tech Library
SOLUTION GUIDES / SOLUTION GUIDES
Okt. 2024
Solution Guide

How to use the "YFF Series" 3-Terminal Feed-through filter for noise suppression and reducing the number of MLCCs

As electronic devices become faster and operate at higher frequencies, capacitors used for noise filtering and decoupling applications require even lower ESL (Equivalent Series Inductance) characteristics.
Additionally, in automotive electrical systems, there is an increasing demand for low-ESL type products to improve safety and comfort and to meet the demands of infotainment.
This Solution Guide introduces various solutions utilizing TDK's advanced low-ESL components, the "YFF Series" 3-terminal feed-through filter.

Structure of the 3-Terminal Feed-Through Filter

The appearance and internal structure of the 3-terminal feed-through filter are illustrated in the conceptual diagram.
Although it is generally called ""3-terminal"", it is actually composed of two terminal electrodes and two ground electrodes. It has an internal structure in which internal electrodes for conduction and internal electrodes for grounding are alternately layered.

Appearance

Terminal electrode Terminal electrode Ground electrode Ground electrode

Noise current path image

:Noise current

Internal structure (schematic diagram)

Internal electrode
for power supply
Internal electrode for
grounding

The feed-through structure shortens the distance between the capacitor and the ground, resulting in lower ESL and enhanced noise suppression.
The parallel effect of two ground electrodes further reduces ESL.

Fig. 1: Conceptual Diagram of the External and Internal Structure of a 3-Terminal Feed-through Filter

Comparison of Impedance-Frequency Characteristics with Other MLCCs

Capacitors for reducing high-frequency noise must have a low ESR (Equivalent Series Resistance) and ESL, as well as a higher SRF (Self Resonant Frequency).
ESR and ESL are influenced by the resistance and inductance of terminal electrodes and internal electrodes.
Therefore, a reverse geometry capacitor, in which a low ESL is achieved by reversing the longitudinal direction and width direction of the terminal electrodes of a normal 2-terminal multilayer ceramic chip capacitor (MLCC) to make the current route wider and shorter, is also effective as a noise countermeasure.
TDK's YFF series 3-terminal feed-through filter achieves even lower ESR and ESL compared to these reverse geometry capacitors.
Figure 2 shows a comparison of the impedance-frequency characteristics and ESL values of TDK's 2-terminal MLCC, reverse geometry capacitor, and the 3-terminal feed-through filter.

Standard 2-terminal MLCC Reverse geometry capacitor 3-terminal feed-through filter
about 200~300pH about 80~100pH about 20~30pH

The ESL value of the 3-terminal feed-through filter is lower compared to standard 2-terminal MLCCs and reverse geometry capacitors.

Fig. 2: Comparison of impedance and ESL values by structure

Applications and Expected Effects of 3-Terminal Feed-Through Filters

We will introduce solution examples for decoupling, filter, and DC/DC converter applications.

Solution Example for Decoupling Application

Voltage fluctuations in the power supply line can destabilize circuit operation and cause noise. To address this, a capacitor is inserted between the power supply line and ground, providing a temporary supply of current to suppress voltage fluctuations when the load changes suddenly.
This is known as decoupling, and the capacitors used for this purpose are called decoupling capacitors.
In recent years, the number of decoupling capacitors required to clear the target impedance has been increasing due to the higher power consumption, higher frequencies, and lower voltages associated with the miniaturization of SoCs. The YFF series 3-terminal feed-through filter, characterized by low ESL, is effective in reducing the number of capacitors needed when replacing conventional 2-terminal capacitors.

Impedance Comparison

2-terminal MLCC/
1005mm(0402inch)/1uF (1pc)
2-terminal MLCC/1005mm(0402inch)
1uF/100nF/10nF/1nF (4pcs)
3-terminal feed-through filter/
1005mm(0402inch)/1µF (1pc)

The effect of reducing the number of
components can be observed.

Fig. 3: Impedance Comparison

We will demonstrate a reduction in the number of components using a 3-terminal feedthrough filter for decoupling applications using a PI simulation.
Here, we compare impedance data as seen from the SoC side.
A common feature between the configurations before and after the proposal is that three 22uF MLCCs are connected to the DC/DC converter for smoothing.

Circuit Image

Current Configuration and TDK Proposed Configuration

Current configuration

2-terminal 1005mm (0402inch) x 24pcs

TDK proposed configuration

3-terminal 1608mm (0603inch) x 3pcs
3-terminal 1005mm (0402inch) x 4pcs

Fig. 4: Circuit image and layout of current and TDK proposed configurations
Current configuration TDK proposed configuration

The current configuration and the TDK proposed configuration have almost the same characteristics.

Fig. 5: Comparison of impedance data between current configuration and TDK proposed configuration

Current configuration

Terminal Structure Product Type
(mm/inch)
Capacitance
(uF)
Quantity
(pcs)
Total Capacitance
(uF)
Mounting Area
(mm2)
2-terminal 1005/0402 1 16 16 8
2-terminal 1005/0402 0.1 8 0.8 4
Current Configuration 24 16.8 12

Number of components: -17pcs,
Mounting area: -51%

TDK proposed configuration

Terminal Structure Product Type
(mm/inch)
Capacitance
(uF)
Quantity
(pcs)
Total Capacitance
(uF)
Mounting Area
(mm2)
3-terminal 1608/0603 4.7 3 14.1 3.84
3-terminal 1005/0402 1 4 4 2
TDK's Proposed Configuration 7 18.1 5.84

Replacing a 2-terminal MLCC with a 3-terminal feed-through filter is expected to reduce the number of components. However, in actual circuits, the electrical elements of the board pattern are added, so the optimal number of decoupling capacitors may vary depending on the board layout.
TDK offers a free simulation service for replacing with a 3-terminal feed-through filter through PI simulation. For more details, please contact us.

Fig. 6: Comparison of number of components and mounting area

Solution Example for Filter Application

With the recent increase in the operating frequency of power ICs, high-frequency noise has become a problem, causing abnormal operation of the set.
As a common countermeasure, a C-L-C π-type filter is configured on the power line.
However, incorporating a 3-terminal feed-through filter into the filter's capacitor can achieve a higher attenuation effect.
Figure 8 shows the results of transfer characteristics obtained through simulation, while Figure 9 presents the conducted noise (voltage method) measured in different noise modes using the actual DC/DC converter.
Please note that for the conducted noise voltage method in Figure 9, measurements were taken in all three configurations with our common mode filters installed as a common mode countermeasure.

Measurement Conditions and Circuit Diagram

Π-type filter configuration 1 2 3
Wiring image
* No filter
C1 - 2-terminal capacitor,
3216mm(1206inch) ,
4.7uF , 35V
3-terminal feed-through filter
3216mm(1206inch) ,
1uF , 100V , 6A
YFF31AH2A105M
Feed-through connection*
L1 - Ferrite bead
2.0×1.2mm,
220Ω at 100MHz, 3A
Ferrite bead
2.0×1.2mm,
220Ω at 100MHz, 3A
C2 - 2-terminal capacitor,
3216mm(1206inch) ,
4.7uF , 35V
3-terminal feed-through filter
3216mm(1206inch) ,
1uF , 100V , 6A
YFF31AH2A105M
Feed-through connection*

*Please refer to the link below for Shunt-through connection.
About connection method

Fig. 7: Measurement conditions and circuit diagram

*The insertion loss includes the filter +
2-terminal MLCC 4.7uF + 2-terminal MLCC 0.1uF.

Insertion Loss Comparison

82MHz comparison

Configuration 1:-43dB

Configuration 2:-87dB

Configuration 3:-151dB

-44dB -64dB

Incorporating a 3-terminal feed-through filter
achieves a high attenuation characteristic.

Configuration 1: No filter

Configuration 2: Capacitors (2-terminal)

Configuration 3: 3-terminal feed-through filter

Fig. 8: Insertion loss comparison

Normal Mode

Normal mode noise is found to be high in
the evaluation environment of this DC/DC converter.

82MHz comparison

Configuration 1:54dBuV/m

Configuration 2:30dBuV/m

Configuration 3:20dBuV/m

-24dB -10dB

Especially in normal mode noise, incorporating a 3-terminal feed-through filter achieves a high noise reduction effect.

Configuration 1: No filter

Configuration 2: Capacitors (2-terminal)

Configuration 3: 3-terminal feedthrough filter

Common Mode

Common Mode + Normal Mode

By incorporating a 3-terminal feed-through filter into the filter, a high attenuation effect can be achieved over a wide frequency range.

Fig. 9: Measured results of each noise mode

Solution Examples for DC/DC Converter Applications

The switching frequency of the DC/DC converter has been increased from the conventional several hundred kHz to over 2 MHz,
as shown below, in order to reduce component size, obtain faster response, and avoid interference with the AM radio frequency band.
As a result, the frequencies of ripple noise and ringing noise are also increasing, creating a demand for broadband noise suppression measures up to the high frequency range of several hundred MHz.
In this case study, we introduce the effects of using 3-terminal feedthrough filters on both the input and output sides of the DC/DC converter to suppress power fluctuations and reduce the number of components.

Example of a 3-terminal feed-through filter placed near the input terminal of a DC/DC converter

The input terminal of the DC/DC converter can generate significant high-frequency noise due to switching noise from wiring and IC parasitic components, leading to Nth-order harmonics from the fundamental frequency. This noise may radiate into external circuits. To address this, it is usually necessary to suppress the noise at its source, often by placing a small ceramic capacitor near the IC. Here, we present an example of a DC/DC converter using a 3-terminal feed-through filter. In this design, the 3-terminal feed-through filter is used as a noise countermeasure close to the IC. Both configurations include a 2-terminal MLCC 10uF capacitor placed on both sides of the input terminal.

DC/DC converter conditions Input voltage: 5V Output voltage: 0.8V Switching frequency:2MHz Output current: 4A
Configuration 2-terminal MLCC
1005mm/0402inch, 100nF,50V
x 1pc
*Shunt-through connection
3-terminal feed-through Filter
YFF18AC1A104M
1608mm/0603inch , 100nF ,10V
x 1pc
*Shunt-through connection
Wiring image

One side of power supply connected on the inner layer

Circuit diagram image

*Please refer to the link below for Shunt-through connection.
About connection method

Fig. 10: Circuit diagram and wiring image

Voltage Waveform Comparison

2-terminal
0.1uFx1pc
1.64Vpp

3-terminal
0.1uFx1pc
0.92Vpp

-0.72V

Conducted Noise Comparison

2-terminal
0.1uFx1pc
65dBuVmax

3-terminal
0.1uFx1pc
60dBuVmax

-5dB

The 3-terminal is effective in suppressing voltage fluctuations and noise levels.

Fig. 11: Comparison of voltage waveforms and conducted noise (100MHz-1GHz)

Example of a 3-terminal feed-through filter placed on the output side of a DC/DC converter

On the output side of a DC/DC converter, significant high-frequency noise can also be generated due to Nth harmonics from the fundamental frequency and parasitic components of wiring and ICs, which can radiate to external circuits.
With the reduction in SoC voltage, the margin between maximum and minimum voltage has decreased. Additionally, as devices become more functional, more systems are becoming sensitive to high-frequency noise. In addition to addressing the issue on the SoC side, it is considered desirable to implement countermeasures on the power supply IC side, which is the source of the noise. Conventionally, an effective method for noise suppression was to arrange multiple 2-terminal MLCCs in stages. However, here we introduce an example where power supply fluctuations can be suppressed by using TDK's large-capacity 3-terminal feed-through filter. Both configurations include a 2-terminal MLCC 47uF capacitor as the output capacitor.

Configuration 2-terminal MLCC
1608mm/0603inch, 1uF, 16V
x 5pcs
3-terminal feed-through filter
YFF18AC0G106M
1608mm/0603inch, 10uF, 4V
x1 pc
*Shunt-through connection
3-terminal feed-through filter
YFF18AC0G106M
1608mm/0603inch, 10uF, 4V
x3 pcs
*Shunt-through connection
DC/DC Converter conditions Input voltage: 5V Output voltage: 1.8V Switching frequency: 2MHz Output current: 2A
Wiring image
Circuit diagram image
Fig. 12: Circuit diagram and wiring image

Insertion Loss Comparison

2-terminal
1uFx5pcs
-48.4dB

3-terminal
10uFx1pc
-50.5dB

3-terminal
10uFx3pcs
-65.9dB

(100MHz comparison) -2.1dB -15.4dB

Voltage Waveform Comparison

2-terminal
1uFx5pcs
19mVpp

3-terminal
10uFx1pc
15mVpp

3-terminal
10uFx3pcs
5mVpp

-4mV -10mV

The 3-terminals provide a high attenuation effect, making it effective for reducing the number of components and improving characteristics.
By connecting multiple 3-terminals in parallel, a high attenuation effect can be achieved.p

Fig. 13: Comparison of insertion loss and voltage waveform

The voltage waveform focuses on switching noise.
By increasing the number of 3-terminal feed-through filters in parallel from one to three, switching noise was almost entirely eliminated.

Voltage Waveform Comparison

By incorporating TDK’s large-capacity 3-terminal feed-through filter, the amplitude level can be suppressed, effectively reducing the number of components.
Additionally, increasing the number of 3-terminal filters in parallel enhances the attenuation effect.
In this case, high-frequency switching noise was nearly eliminated with three parallel 3-terminal filters in Configuration 3.

Fig. 14: Effect of increasing the number of 3-terminal feed-through filters on switching noise rejection

Important Points to Fully Utilize the Characteristics of the 3-Terminal Feed-Through Filter

3-terminal feed-through filters are characterized by low ESL when used individually, but to fully utilize this feature, it is important to reduce parasitic components from ground patterns and vias.
Figure 15 shows the relationship between the length (depth) of the through-hole connecting the ground pattern and ground plane and the attenuation-frequency characteristics of the 3-terminal feed-through filter.

Simulations were performed to compare the following mounting conditions ① to ③.

When there are two through-holes at both ends of the ground pattern (condition ①) versus one through-hole on one side (condition ②), the configuration with two through-holes on both sides shows a greater attenuation. Additionally, with two through-holes on both sides and deeper through-holes (condition ③), the configuration with shorter (shallower) through-holes (condition ①) shows a greater attenuation.

Standalone 3-terminal feed-through filter characteristics YFF15AC0J105M (1005mm(0402inch)/6.3V/1uF)

Condition ① Condition ② Condition ③

To fully utilize the characteristics of the 3-terminal feed-through filter, it is recommended to use multiple GND terminal through-holes and keep the through-hole length (depth) short.

Fig. 15: Relationship between the length (depth) of through-holes connecting the ground pattern and ground plane and the attenuation-frequency characteristics of the 3-terminal feed-through filter

Connection Methods

3-terminal Feed-through filters are typically used connected to the power line, and there are two connection methods.
As shown in Figure 16, these methods are series connection (feed-through connection) and parallel connection (shunt-through connection).
The figure below illustrates each connection example. In this example, the first inner layer of the multilayer printed circuit board is the ground plane layer, and the second inner layer is the power line layer, with vias connecting each plane. For feed-through connection, a part of the power line pattern is cut and mounted, whereas for shunt-through connection, the power line pattern is is mounted without cutting.
Please refer to the table summarizing the characteristics and main applications of each connection method.

Fig. 16: Comparison of feed-through connection and shunt-through connection
  Feed-through connection Shunt-through connection
Mounting method Cut a portion of the line pattern where noise
needs to be removed and insert the filter.
Mount parallel (shunt) connection without
cutting the line wiring pattern.
Main applications Noise removal in high-frequency bands
(filter applications)
Suppression of IC voltage fluctuation
(decoupling applications)
Advantages High noise removal effectiveness over a wide band up to high frequencies. No rated current limitation as almost no current flows through the chip.
Easy to change the number of components even after board
design, as the wiring pattern is not cut.
Disadvantages Rated current limitation due to current flowing
through the chip. Design changes are difficult
because the power line/signal line is cut.
Slightly higher ESL compared to feed-through connection.
Noise removal
effectiveness
Effectively dissipates noise to GND as noise on
the line must pass through the chip.
Some noise passes through the power line, making noise removal
less effective compared to feed-through connection.
Voltage fluctuation
suppression effect

(Voltage drop occurs.)

(Smaller voltage drop.)

Choose the appropriate mounting method according to the application.

In a feed-through connection, the voltage drop is greater than in a shunt-through connection, but the noise removal effect is higher. On the other hand, shunt-through connections can suppress voltage drops in the power line, making them suitable for low-voltage circuits. Please refer to the comparison table and select the connection method that best suits your application.

Fig. 17: Comparison of simulated load fluctuation between feed-through and shunt-through connections (image)

Conclusion

The YFF series 3-terminal feed-through filter is characterized by low ESL and high noise removal effectiveness. Due to its expanding lineup of high-capacity products, it is increasingly in demand for reducing component count and improving characteristics in filter applications, DC/DC converter applications, and decoupling applications

TDK offers products with a wide range of rated voltages and capacitances, enabling comprehensive product proposals from the power supply’s input side to the output side.
However, as demonstrated, the characteristics can vary depending on the board pattern and connection method. If you need support in using these products or are interested in PI simulation, please contact TDK.

For inquiries related to our products or sales, please contact us by filling the following Contact Form.

Contact

Please click here for information on the list of distributors.

Related Links