Applications & Cases
Application Note
Ag-Stacked Transparent Conductive Film
TDK's transparent conductive silver [Ag] alloy film (FleClear®) is a versatile material that has numerous use cases. Many of these uses require making direct electrical contact to the film's low resistance conductive surface in order to adequately perform the targeted applications. The following Application Note provides an overview of FleClear®, a step-by-step procedure of attaching an metal electrode, a list of needed equipment, along with the recommended materials to attach copper bus bars to the conductive surface. Additionally, where important, the suppliers and the respective numbers, are also listed..
Read more