Q.
Why should I use these technical support tools?
- Capacitors /
- Inductors (Coils) /
- EMC Components /
- RF Components /
- Voltage / Current / Temperature Protection Devices /
- Transformers >
- Multilayer Ceramic Chip Capacitors /
- 3-Terminal Feedthrough MLCCs /
- Chip Beads /
- 3-terminal Filters /
- Common Mode Filters / Chokes /
- Noise Suppression Filters /
- Baluns /
- Dividers / Splitters /
- Chip Varistors / Ceramic Transient Voltage Suppressors /
- Pulse Transformers and Modules for LAN
A. Recently, electrical circuits designs use simulation technology. In order to improve simulation accuracy, it is very important to acquire a simulation model that is as close as possible to the actual usage. For example, when a 1uF capacitor is used, ESR (Equivalent Series Resistance) and ESL (Equivalent Series Inductance) differ depending on the size. Therefore, if you create a circuit using the ideal capacitor determined by simulation, actual results may be very different. By using a simulation model, you can attain results that are as close as possible to actual phenomena.