FAQ
Q.
Is it a problem if the load currents of each output are not equal in ±2 output products with insulated onboard power supplies?
  • Power Supplies and Loads
  • >
  • DC-DC Converters
  • /
  • AC-DC Power Supplies


A. Please note that the output voltages can fluctuate significantly. The output voltages can be stabilized by controlling the voltages between +Vout and -Vout in circuits such as the one shown in the Figure below as±2 output products are compact.

Figure 1

Figure 1
The output voltages fluctuate with the current values of each output because each output voltage does not undergo stabilized controlling individually. We recommend use combined with a single-output converter when load currents of each output are unequal and precise output voltages are required.