FAQ
Q.
What happens during use if the sensing wires are accidentally left open?
  • Power Supplies and Sources
  • >
  • DC-DC Converters
  • /
  • AC-DC Power Supplies


A. The output voltage cannot be controlled and the voltage increases if the +V and +S along with the -V and -S of the power supply are open.
This starts the overvoltage protection function and interrupts the output. Therefore, please short the areas between the +V and +S as well as the -V and -S using the accompanying parts when not using the remote sensing function.