FAQ
Q.
Can power modules / on-board power supplies be operated just by connecting input-output terminals to power supplies and load devices?
  • Power Supplies and Loads
  • >
  • DC-DC Converters
  • /
  • AC-DC Power Supplies


A. There are power supplies that cannot be operated just by connecting input-output terminals to power supplies and load devices. Please be sure to note the following precautions.
- Products with sensing functions require the sensing terminals to be connected with the output sides.
- Products with remote ON/OFF control functions sometimes require connections with the -Vin terminals or +Vin terminals.
- Some products require peripheral components such as capacitors or choke coils.
Refer to the instruction manuals and basic connections of the respective products for details.