Q.
What is the switching frequency of the CSS Series (CSS65/CSS65A/CSS150CSS500)?
- Power Supplies and Loads >
- AC-DC Power Supplies
Figure 1
A.
The CSS65 has a switching frequency of 63kHz.
The CSS65A has a variable frequency of between 48kHz and 68kHz at full load 115V-230VAC input.
The CSS150 has a variable switching frequency depending on load. (Figure 1)
The CSS500 has a switching frequency of 90 to 100kHz.
Figure 1
Related Information