FAQ
Q.
Is it OK to use the isolated DC-DC converter as non-insulated? What is the connection method in this case?
  • Power Supplies and Loads
  • >
  • DC-DC Converters


A. Yes, it is OK. For information on the connection method, please refer to the example connection application given below.

Figure 1