FAQ
Q.
Is it safe to ground the output on one side?
  • Power Supplies and Loads
  • >
  • AC-DC Power Supplies
  • /
  • DC-DC Converters

A.Basically, it won’t cause a problem with the operation of the power supply, but there is a possibility that the output ripple may worsen and EMC standards may not be met.
Therefore, please evaluate the product thoroughly before use. The insulation withstand voltage specification is eliminated, and the insulation withstand voltage between input and output is the same as that between input and FG.