Q.
Is there a startup time limit?
- Power Supplies and Sources >
- AC-DC Power Supplies /
- DC-DC Converters
A.The startup time from the time of power input to the time when the output voltage rises is not usually specified in the specifications.
The Evaluation Data is available for each model, and the startup time can be read as typical data from the output voltage rise characteristics. The ON/OFF CNT function is also available.
The startup time by ON/OFF CNT for power supplies with ON/OFF CNT function is also available in the Evaluation Data. The ON/OFF CNT output voltage rise characteristics of the Evaluation Data can be referenced as representative data.
Related Information