FAQ
Q.
How many crimp terminals can be connected to one terminal block (one stud)?
  • Power Supplies and Loads
  • >
  • AC-DC Power Supplies
  • /
  • DC-DC Converters

A.Refer to the user manual.
If there is no information in the manual, please consider the following points and make a decision accordingly:
・Ensure the effective screw length allows for proper tightening.
・Prevent contact between different electrical potentials.
・Ensure the connected wires can handle the allowable current.
・Ensure that there is no gap between crimp terminals to prevent an increase in contact resistance.