FAQ
Q.
How does temperature affect the measurement?
  • Sensors and Sensor Systems
  • >
  • Ultrasonic Sensors
  • >
  • Ultrasonic Sensor Disks
  • /
  • Ultrasonic ToF (Time-of-Flight) Sensors


A. The speed of sound in air depends on the temperature and can be approximated as c = 331 m/s + 0.6 * T. Since the output signal of the sensor is the time of flight, the temperature should be compensated.