Q.
Why do some limit temperature sensors have 2 sensing points?
- Sensors and Sensor Systems /
- Voltage / Current / Temperature Protection Devices >
- Temperature Protection Devices /
- Temperature Sensors (PTC) >
- PTC Limit Temperature Sensors (Sensor)
A. The benefit of 2 sensing points is that the first one can be used as a warning signal whereas the second sensig point is used as switch-off criteria to protect the components from over-temperature events.