Ferrite Product Map & Selection Guide
Ferrite is a magnetic material that fundamentally supports the modern electronics society. Applications include Main Transformers, Chokes, EMC, and Communications Equipment.
We offer a wide range of MnZn ferrites tailored to meet the specific characteristics required by our customers. The Product Map in this article shows the material properties of multiple ferrite products. You can also use the Selection Guide to select the optimal ferrite material according to your application.

High-Power Mn-Zn Ferrite PEL95 Material
With the increasing adoption of renewable energy and EV fast-charging stations, the demand for high-power power supplies is growing.
Transformers used in power supplies are expected to be smaller, more efficient, and generate less heat. In order to meet these demands, we developed the PEL95 material, which exhibits low core loss characteristics across a wide temperature range in large cores.
This article introduces the features of the PEL95 material, developed specifically for high-power applications, and key considerations for its use.

High-Temperature Low-Loss
Mn-Zn Ferrite PEM95 Material
With the increasing adoption of renewable energy and the proliferation of EV fast-charging stations, the demand for high-power power supplies is growing.
Transformers used in these power supplies are expected to be more compact, efficient, and generate less heat. In order to meet these demands, we developed the PEM95 material, which reduces core loss at high temperatures in large, high-load conditions.
This article introduces the features of the PEM95 material, developed specifically for high-power applications, and key considerations for its use.

myTDK Members-Only Service
myTDK is a members-only service operated by TDK.
Registration and use are free of charge. Registered members can receive our email newsletter service, view members-only contents, and use other services.

Members-only articles

Collective download of materials