Tech Library Applications & Cases Facet Tech Note List Article Category » Taxonomy term » Name Anechoic Chambers and Radio Wave Absorbers Capacitors Ceramic Switching / Heating, Piezo Components, Contactors, Buzzers and Microphones EMC Components Ferrites and Accessories Inductors (Coils) Noise Suppressing / Magnetic Sheets RF Components Sensors and Sensor Systems Solid-State Batteries Transformers (-) Transparent Conductive Film Voltage / Current / Temperature Protection Devices Wireless Power Transfer Facet Tech Note List Product Categories L1 Automotive Consumer Electronics ICT Industrial & Energy Medical & Healthcare Others Wearables Facet Tech Note List Application Category 2021 2019 Facet Tech Note List Published on Date Applications & Cases Nov. 2021 [Application Note] Ag-Stacked Transparent Conductive Film TDK's transparent conductive silver [Ag] alloy film (FleClear®) is a versatile material that has numerous use cases. Many of these uses require making direct electrical contact to the film's low resistance conductive surface in order to adequately perform the targeted applications. The following Application Note provides an overview of FleClear®, a step-by-step procedure of attaching an metal electrode, a list of needed equipment, along with the recommended materials to attach copper bus bars to the conductive surface. Additionally, where important, the suppliers and the respective numbers, are also listed.. TDK's transparent conductive silver [Ag] alloy film (FleClear®) is a versatile material that has numerous use cases. Many of these uses require making direct electrical contact to the film's low resistance conductive surface in order to adequately perform the targeted applications. The following Application Note provides an overview of FleClear®, a step-by-step procedure of attaching an metal electrode, a list of needed equipment, along with the recommended materials to attach copper bus bars to the conductive surface. Additionally, where important, the suppliers and the respective numbers, are also listed.. Transparent Conductive Film Applications & Cases Nov. 2019 [Application Note] Devices that Enhance the Safety of the Digital Cockpit The methods of use of automobiles will change substantially in the future including autonomous driving and car sharing services, and the human machine interface (HMI) between drivers and their cars will also completely change. The automobile industry is developing the digital cockpit in pursuit of an HMI that will provide safety and reassurance while freeing drivers from the burdens of driving and allow time to be used meaningfully and in comfort. Below is an introduction to TDK product and technologies that enhance the value of the digital cockpit with the aim of achieving an HMI that ensures and enhance safety and reassurance through the driver's senses. The methods of use of automobiles will change substantially in the future including autonomous driving and car sharing services, and the human machine interface (HMI) between drivers and their cars will also completely change. The automobile industry is developing the digital cockpit in pursuit of an HMI that will provide safety and reassurance while freeing drivers from the burdens of driving and allow time to be used meaningfully and in comfort. Below is an introduction to TDK product and technologies that enhance the value of the digital cockpit with the aim of achieving an HMI that ensures and enhance safety and reassurance through the driver's senses. Ceramic Switching / Heating, Piezo Components, Contactors, Buzzers and Microphones Transparent Conductive Film Piezoelectric actuators for haptic feedback MEMS Microphones (Microphone) PiezoHapt™ Actuators PiezoListen™ Piezo Speakers PowerHap™ Actuators