Tech Library
Applications & Cases
[Application Note]
High energy, reliable and volumetric efficient inverters are essential to reducing emissions of vehicles based on 48 V technology. DC-link capacitors can significantly contribute to this target by reducing parasitic losses and increasing thermal efficiency. High inverter powers can be theoretically achieved with multiple capacitor connections. However, a high number of parallel-connected parts also increase the complexity of the system stability. In the field of Aluminum Electrolytic Capacitors, the Hybrid Polymer technology offers higher ripple current densities by a factor of, e.g., 5x compared to standard Liquid Electrolyte technology. By applying the Hybrid Polymer technology to the large axial capacitor can sizes, with solid mechanical construction and special thermal dissipation feature, a compact DC-link solution with a reduced amount of capacitor and minimized thermal escalation risk through stable and efficient thermal design can be achieved.
High energy, reliable and volumetric efficient inverters are essential to reducing emissions of vehicles based on 48 V technology. DC-link capacitors can significantly contribute to this target by reducing parasitic losses and increasing thermal efficiency. High inverter powers can be theoretically achieved with multiple capacitor connections. However, a high number of parallel-connected parts also increase the complexity of the system stability. In the field of Aluminum Electrolytic Capacitors, the Hybrid Polymer technology offers higher ripple current densities by a factor of, e.g., 5x compared to standard Liquid Electrolyte technology. By applying the Hybrid Polymer technology to the large axial capacitor can sizes, with solid mechanical construction and special thermal dissipation feature, a compact DC-link solution with a reduced amount of capacitor and minimized thermal escalation risk through stable and efficient thermal design can be achieved.
Products & Technologies
[Product Overview]
TDK, a world leader in material technologies, manufacturing and electronic components, has recently developed and released a state-of-the-art, Qi compliant planar wireless power coil utilizing a unique copper patterning technology that provides multiple end-user benefits. The Wireless Power Consortium [WPC] has designated this new coil as MP-A28, while the corresponding TDK part number is WCT38466-N0E0SST01. TDK’s “pattern coil” technology allows for intricate coil patterns that cannot be duplicated by the use of discrete wires and yields tight trace width and gap control normally associated with the finest etching processes and technologies. Also unique to TDK’s technology, is the ease and flexibility to accurately change the copper trace thickness, depending on the application requirements, which is not available by traditional copper coil techniques.
TDK, a world leader in material technologies, manufacturing and electronic components, has recently developed and released a state-of-the-art, Qi compliant planar wireless power coil utilizing a unique copper patterning technology that provides multiple end-user benefits. The Wireless Power Consortium [WPC] has designated this new coil as MP-A28, while the corresponding TDK part number is WCT38466-N0E0SST01. TDK’s “pattern coil” technology allows for intricate coil patterns that cannot be duplicated by the use of discrete wires and yields tight trace width and gap control normally associated with the finest etching processes and technologies. Also unique to TDK’s technology, is the ease and flexibility to accurately change the copper trace thickness, depending on the application requirements, which is not available by traditional copper coil techniques.
Applications & Cases
[Application Note]
Service robots play an increasingly vital role in society, from transportation and warehouse logistics to home entertainment and security. Regardless of their application, they need to sense changes in their surroundings in real-time to ensure safety while providing a positive user experience. To illustrate how various sensor technologies from TDK’s SmartSensor family can be applied in service robots, this article focuses on a robotic vacuum cleaner (RVC).
Early versions of robotic vacuums had very little intelligence, randomly bumping their way around the home and sometimes missing areas as they did not know where they had been. Often, they would unwittingly become trapped or run out of charge mid-sweep. And, as their dust box is comparatively small to a regular vacuum cleaner, if full, they could be sweeping but not collecting anything up. Over the years, with the innovative use of sensors and motor controllers, vacuum cleaning robots have become much smarter, overcoming these issues.
Service robots play an increasingly vital role in society, from transportation and warehouse logistics to home entertainment and security. Regardless of their application, they need to sense changes in their surroundings in real-time to ensure safety while providing a positive user experience. To illustrate how various sensor technologies from TDK’s SmartSensor family can be applied in service robots, this article focuses on a robotic vacuum cleaner (RVC).
Early versions of robotic vacuums had very little intelligence, randomly bumping their way around the home and sometimes missing areas as they did not know where they had been. Often, they would unwittingly become trapped or run out of charge mid-sweep. And, as their dust box is comparatively small to a regular vacuum cleaner, if full, they could be sweeping but not collecting anything up. Over the years, with the innovative use of sensors and motor controllers, vacuum cleaning robots have become much smarter, overcoming these issues.
Products & Technologies
[Product Overview]
The TDK Robokit1 combines sensors, processors, and actuators on a single board, making it an ideal robotics platform for quick prototyping and development. RoboKit1 integrates key product offerings such as 6-axis IMU, industrial IMU modules, capacitive barometric pressure sensor, digital I²S microphone, temp sensor, ultrasonic Time of Flight (ToF) sensors, magnetometer, and motor controller on a single PCB.
It also comes equipped with ARM® Cortex®-M7, multiple interfaces, and is compatible with multiple processor platforms such as Raspberry Pi and ASUS Tinker Board. RoboKit1 is not just another dev board—it is the comprehensive TDK solution showcase!
The TDK Robokit1 combines sensors, processors, and actuators on a single board, making it an ideal robotics platform for quick prototyping and development. RoboKit1 integrates key product offerings such as 6-axis IMU, industrial IMU modules, capacitive barometric pressure sensor, digital I²S microphone, temp sensor, ultrasonic Time of Flight (ToF) sensors, magnetometer, and motor controller on a single PCB.
It also comes equipped with ARM® Cortex®-M7, multiple interfaces, and is compatible with multiple processor platforms such as Raspberry Pi and ASUS Tinker Board. RoboKit1 is not just another dev board—it is the comprehensive TDK solution showcase!
Products & Technologies
[Product Training Module]
The electrification of automobiles is advancing toward autonomous driving, and accordingly noise countermeasures in automobiles become increasingly important. This time, we will introduce an automotive noise suppression filter MHF/MDF series that has unique features as compared to general chip beads.
The MHF series achieves a high impedance in the MF and HF bands ranging from 300 kHz to 30 MHz used in radios, etc., and has an excellent noise suppression effect. Furthermore, the MDF series is a product with excellent DC bias characteristics of impedance so that an excellent noise suppression effect can be obtained even when used in a power supply line.
*Registration and login to myTDK is required to view this content.
The electrification of automobiles is advancing toward autonomous driving, and accordingly noise countermeasures in automobiles become increasingly important. This time, we will introduce an automotive noise suppression filter MHF/MDF series that has unique features as compared to general chip beads.
The MHF series achieves a high impedance in the MF and HF bands ranging from 300 kHz to 30 MHz used in radios, etc., and has an excellent noise suppression effect. Furthermore, the MDF series is a product with excellent DC bias characteristics of impedance so that an excellent noise suppression effect can be obtained even when used in a power supply line.
*Registration and login to myTDK is required to view this content.